# Get zone set configuration metadata

GET http://os-992244000006.local/api/v1/zone_monitor/{zone_set}

Returns the complete zone set metadata including version, zones configuration, power-on live IDs, and sensor-to-body transform. Zone configurations include file hashes and coordinate frames.

Reference: https://docs.ouster.com/sensor-docs/firmware/api-reference/ouster-http-api/zone-monitor/get-zone-set-configuration-metadata

## Request

### Path parameters

- `zone_set` (enum, required) — Zone set identifier. Valid values are 'active' or 'staged'. The 'pending' set is a transient state and should not be used.
  - Allowed values: `active`, `staged`

## Response

### 200

Zone set metadata with enriched zone information

- `version` (ZoneSetConfigVersion, required)
- `power_on_live_ids` (list of integer, required) — List of power-on live zone IDs (max 16). Must be non-empty when zones are configured.
- `zones` (ZoneSetConfigZones, required) — Zone configurations (at least one zone required per schema)
- `label` (string, optional) — Optional label for the zone set
- `sensor_to_body_transform` (list of double, optional) — 4x4 transformation matrix as a flat array of 16 elements

## Errors

### 404 Not Found Error

Zone set not found

- `any`

## Types

### ZoneSetConfigVersion

### ZoneSetConfigZones

Zone configurations (at least one zone required per schema)

## Examples

**Response**

```json
{
  "version": {
    "file_naming": 7,
    "metadata": 12
  },
  "power_on_live_ids": [
    3,
    7,
    12
  ],
  "zones": {
    "3": {
      "coordinate_frame": "sensor",
      "file_hash": "a3f5c9d8e7b4f2a1c6d8e9f0b1a2c3d4",
      "frame_count": 5,
      "mode": "OCCUPANCY",
      "point_count": 15
    },
    "7": {
      "coordinate_frame": "body",
      "file_hash": "b1c2d3e4f5a6b7c8d9e0f1a2b3c4d5e6",
      "frame_count": 3,
      "mode": "VACANCY",
      "point_count": 10
    },
    "12": {
      "coordinate_frame": "sensor",
      "file_hash": "c4d5e6f7a8b9c0d1e2f3a4b5c6d7e8f9",
      "frame_count": 7,
      "mode": "OCCUPANCY",
      "point_count": 20
    }
  },
  "label": "Warehouse Zone Set A",
  "sensor_to_body_transform": [
    1,
    0,
    0,
    0,
    0,
    0.866,
    -0.5,
    0,
    0,
    0.5,
    0.866,
    0,
    0.1,
    0.2,
    0.3,
    1
  ]
}
```

**SDK Code**

```python
import requests

url = "http://os-992244000006.local/api/v1/zone_monitor/active"

response = requests.get(url)

print(response.json())
```

```javascript
const url = 'http://os-992244000006.local/api/v1/zone_monitor/active';
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
	url := "http://os-992244000006.local/api/v1/zone_monitor/active"
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
url = URI("http://os-992244000006.local/api/v1/zone_monitor/active")
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
HttpResponse<String> response = Unirest.get("http://os-992244000006.local/api/v1/zone_monitor/active")
  .asString();
```

```php
<?php
require_once('vendor/autoload.php');

$client = new \GuzzleHttp\Client();

$response = $client->request('GET', 'http://os-992244000006.local/api/v1/zone_monitor/active');

echo $response->getBody();
```

```csharp
using RestSharp;

var client = new RestClient("http://os-992244000006.local/api/v1/zone_monitor/active");
var request = new RestRequest(Method.GET);
IRestResponse response = client.Execute(request);
```

```swift
import Foundation

let request = NSMutableURLRequest(url: NSURL(string: "http://os-992244000006.local/api/v1/zone_monitor/active")! as URL,