# Set T1 ethernet speed override

PUT http://os-992244000006.local/api/v1/system/network/speed_override
Content-Type: application/json

Set the automotive ethernet (T1) speed override

__Warning:__ Only modify this resource if the link partner can be configured to match (i.e. 1000BASE-T1 or 100BASE-T1), otherwise communication will be lost with the sensor.

Reference: https://docs.ouster.com/sensor-docs/firmware/api-reference/ouster-http-api/system/put-network-speed-override

## Request

### Body (application/json)

This endpoint expects an enum.

- `enum`
  - Allowed values: `100`

## Response

### 200

No error

## Examples

**Request**

```json
"100"
```

**Response**

```json
"100"
```

**SDK Code**

```python
import requests

url = "http://os-992244000006.local/api/v1/system/network/speed_override"

payload = "100"
headers = {"Content-Type": "application/json"}

response = requests.put(url, json=payload, headers=headers)

print(response.json())
```

```javascript
const url = 'http://os-992244000006.local/api/v1/system/network/speed_override';
const options = {method: 'PUT', headers: {'Content-Type': 'application/json'}, body: '"100"'};
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
	"strings"
	"net/http"
	"io"
)

func main() {

	url := "http://os-992244000006.local/api/v1/system/network/speed_override"

	payload := strings.NewReader("\"100\"")

	req, _ := http.NewRequest("PUT", url, payload)

	req.Header.Add("Content-Type", "application/json")
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
url = URI("http://os-992244000006.local/api/v1/system/network/speed_override")

http = Net::HTTP.new(url.host, url.port)

request = Net::HTTP::Put.new(url)
request["Content-Type"] = 'application/json'
request.body = "\"100\""

response = http.request(request)
puts response.read_body
```

```java
import com.mashape.unirest.http.HttpResponse;
import com.mashape.unirest.http.Unirest;

HttpResponse<String> response = Unirest.put("http://os-992244000006.local/api/v1/system/network/speed_override")
  .header("Content-Type", "application/json")
  .body("\"100\"")
  .asString();
```

```php
<?php
require_once('vendor/autoload.php');

$client = new \GuzzleHttp\Client();

$response = $client->request('PUT', 'http://os-992244000006.local/api/v1/system/network/speed_override', [
  'body' => '"100"',
  'headers' => [
    'Content-Type' => 'application/json',
  ],
]);

echo $response->getBody();
```

```csharp
using RestSharp;

var client = new RestClient("http://os-992244000006.local/api/v1/system/network/speed_override");
var request = new RestRequest(Method.PUT);
request.AddHeader("Content-Type", "application/json");
request.AddParameter("application/json", "\"100\"", ParameterType.RequestBody);
IRestResponse response = client.Execute(request);
```

```swift
import Foundation

let headers = ["Content-Type": "application/json"]
let parameters = "100" as [String : Any]

let postData = JSONSerialization.data(withJSONObject: parameters, options: [])

let request = NSMutableURLRequest(url: NSURL(string: "http://os-992244000006.local/api/v1/system/network/speed_override")! as URL,
                                        cachePolicy: .useProtocolCachePolicy,
                                    timeoutInterval: 10.0)
request.httpMethod = "PUT"
request.allHTTPHeaderFields = headers
request.httpBody = postData as Data