# Reset OSSD output

POST http://os-992244000006.local/api/v1/sensor/ossd/reset
Content-Type: application/json

Manually clear latched OSSD trips and faults by cycling the OSSD generator
enable. The request must echo the current `reset_id` from the OSSD status
endpoint; Keeper rotates the token on success so the request cannot be
replayed. Returns the post-reset status, including the new `reset_id`.
A trip source that is still asserted, or a persistent hardware fault,
re-latches immediately.


Reference: https://docs.ouster.com/sensor-docs/firmware/api-reference/ouster-http-api/sensor-metadata/post-ossd-reset

## Request

### Body (application/json)

This endpoint expects an OssdResetRequest.

- `reset_id` (uint, required) — The current `reset_id` from the OSSD status endpoint. Rejected if it does not match the live token.

## Response

### 200

OSSD status after reset

- `configured` (boolean, required) — True when OSSD dual-channel output is configured on the MIO pins
- `status` (enum, required) — Live OSSD generator status. * `DISABLED` - OSSD generator is not running. * `ENABLED` - OSSD generator is enabled. * `ACTIVE` - OSSD outputs are asserted and diagnostics are clean. * `TRIPPED` - outputs are deasserted because the trip source asserted (for example a Zone Monitor infringement). Not a hardware failure. * `FAULT` - OSSD diagnostics detected a defect such as a short, open load, or failed startup qualification.
  - Allowed values: `DISABLED`, `ENABLED`, `ACTIVE`, `TRIPPED`, `FAULT`
- `source` (enum, required) — Selected OSSD trip source
  - Allowed values: `NOT_SET`, `SYSTEM_FAULT`, `ZONE_MONITOR`
- `errors` (list of string, required) — Human-readable latched OSSD trip and fault messages
- `reset_id` (uint, required) — Single-use token that must be echoed by a reset request. Rotated on each successful reset so a stale or replayed request cannot re-clear a latched fault.

## Errors

### 400 Bad Request Error

OSSD is not configured, or the reset_id is missing, invalid, or stale

- `any`

### 500 Internal Server Error

Unexpected response format from sensor

- `any`

## Examples

**Request**

```json
{
  "reset_id": 1
}
```

**Response**

```json
{
  "configured": true,
  "status": "DISABLED",
  "source": "NOT_SET",
  "errors": [
    "string"
  ],
  "reset_id": 1
}
```

**SDK Code**

```python
import requests

url = "http://os-992244000006.local/api/v1/sensor/ossd/reset"

payload = { "reset_id": 1 }
headers = {"Content-Type": "application/json"}

response = requests.post(url, json=payload, headers=headers)

print(response.json())
```

```javascript
const url = 'http://os-992244000006.local/api/v1/sensor/ossd/reset';
const options = {
  method: 'POST',
  headers: {'Content-Type': 'application/json'},
  body: '{"reset_id":1}'
};
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
	"strings"
	"net/http"
	"io"
)

func main() {

	url := "http://os-992244000006.local/api/v1/sensor/ossd/reset"

	payload := strings.NewReader("{\n  \"reset_id\": 1\n}")

	req, _ := http.NewRequest("POST", url, payload)

	req.Header.Add("Content-Type", "application/json")
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
url = URI("http://os-992244000006.local/api/v1/sensor/ossd/reset")

http = Net::HTTP.new(url.host, url.port)

request = Net::HTTP::Post.new(url)
request["Content-Type"] = 'application/json'
request.body = "{\n  \"reset_id\": 1\n}"

response = http.request(request)
puts response.read_body
```

```java
import com.mashape.unirest.http.HttpResponse;
import com.mashape.unirest.http.Unirest;

HttpResponse<String> response = Unirest.post("http://os-992244000006.local/api/v1/sensor/ossd/reset")
  .header("Content-Type", "application/json")
  .body("{\n  \"reset_id\": 1\n}")
  .asString();
```

```php
<?php
require_once('vendor/autoload.php');

$client = new \GuzzleHttp\Client();

$response = $client->request('POST', 'http://os-992244000006.local/api/v1/sensor/ossd/reset', [
  'body' => '{
  "reset_id": 1
}',
  'headers' => [
    'Content-Type' => 'application/json',
  ],
]);

echo $response->getBody();
```

```csharp
using RestSharp;

var client = new RestClient("http://os-992244000006.local/api/v1/sensor/ossd/reset");
var request = new RestRequest(Method.POST);
request.AddHeader("Content-Type", "application/json");
request.AddParameter("application/json", "{\n  \"reset_id\": 1\n}", ParameterType.RequestBody);
IRestResponse response = client.Execute(request);
```

```swift
import Foundation

let headers = ["Content-Type": "application/json"]
let parameters = ["reset_id": 1] as [String : Any]

let postData = JSONSerialization.data(withJSONObject: parameters, options: [])

let request = NSMutableURLRequest(url: NSURL(string: "http://os-992244000006.local/api/v1/sensor/ossd/reset")! as URL,
                                        cachePolicy: .useProtocolCachePolicy,
                                    timeoutInterval: 10.0)
request.httpMethod = "POST"
request.allHTTPHeaderFields = headers
request.httpBody = postData as Data