# Get OSSD output status

GET http://os-992244000006.local/api/v1/sensor/ossd/status

Query the live OSSD dual-channel output status, selected trip source, and any
latched trip or fault messages. OSSD may be driven by Zone Monitor or other
system-fault sources depending on `mio_applications`.


Reference: https://docs.ouster.com/sensor-docs/firmware/api-reference/ouster-http-api/sensor-metadata/get-ossd-status

## Response

### 200

OSSD status

- `configured` (boolean, required) — True when OSSD dual-channel output is configured on the MIO pins
- `status` (enum, required) — Live OSSD generator status. * `DISABLED` - OSSD generator is not running. * `ENABLED` - OSSD generator is enabled. * `ACTIVE` - OSSD outputs are asserted and diagnostics are clean. * `TRIPPED` - outputs are deasserted because the trip source asserted (for example a Zone Monitor infringement). Not a hardware failure. * `FAULT` - OSSD diagnostics detected a defect such as a short, open load, or failed startup qualification.
  - Allowed values: `DISABLED`, `ENABLED`, `ACTIVE`, `TRIPPED`, `FAULT`
- `source` (enum, required) — Selected OSSD trip source
  - Allowed values: `NOT_SET`, `SYSTEM_FAULT`, `ZONE_MONITOR`
- `errors` (list of string, required) — Human-readable latched OSSD trip and fault messages
- `reset_id` (uint, required) — Single-use token that must be echoed by a reset request. Rotated on each successful reset so a stale or replayed request cannot re-clear a latched fault.

## Errors

### 500 Internal Server Error

Unexpected response format from sensor

- `any`

## Examples

**Response**

```json
{
  "configured": true,
  "status": "DISABLED",
  "source": "NOT_SET",
  "errors": [
    "string"
  ],
  "reset_id": 1
}
```

**SDK Code**

```python
import requests

url = "http://os-992244000006.local/api/v1/sensor/ossd/status"

response = requests.get(url)

print(response.json())
```

```javascript
const url = 'http://os-992244000006.local/api/v1/sensor/ossd/status';
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
	url := "http://os-992244000006.local/api/v1/sensor/ossd/status"
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
url = URI("http://os-992244000006.local/api/v1/sensor/ossd/status")
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
HttpResponse<String> response = Unirest.get("http://os-992244000006.local/api/v1/sensor/ossd/status")
  .asString();
```

```php
<?php
require_once('vendor/autoload.php');

$client = new \GuzzleHttp\Client();

$response = $client->request('GET', 'http://os-992244000006.local/api/v1/sensor/ossd/status');

echo $response->getBody();
```

```csharp
using RestSharp;

var client = new RestClient("http://os-992244000006.local/api/v1/sensor/ossd/status");
var request = new RestRequest(Method.GET);
IRestResponse response = client.Execute(request);
```

```swift
import Foundation

let request = NSMutableURLRequest(url: NSURL(string: "http://os-992244000006.local/api/v1/sensor/ossd/status")! as URL,