# Get all Multipurpose IO (MIO) channel states

GET http://os-992244000006.local/api/v1/sensor/mio

Get the current state of all Multipurpose IO (MIO) hardware channels including aliases, configuration, and pin values. MIO channels provide configurable input/output functionality for external hardware integration.

### MIO Channel Availability

The availability of MIO channels is determined by the sensor's `mio_applications` configuration. Each entry selects an application (intent), protocol, pin(s), and optional drive mode. Legacy `mio_functions` and `multipurpose_io_mode` fields are migrated automatically on load.

* __Channel 0 (SYNC_PULSE_IN):__ Available when not assigned by a `TIME_SYNC_INPUT` / `PPS` application.

* __Channel 1 (MULTIPURPOSE_IO):__ Available when not assigned by another `mio_applications` entry. General-purpose runtime control requires a `GENERAL_PURPOSE_IO` / `GPIO` application on that pin.

Reference: https://docs.ouster.com/sensor-docs/firmware/api-reference/ouster-http-api/sensor-metadata/get-mio

## Response

### 200

Multipurpose IO hardware states for all channels

- `input_bitmask` (uint, required) — Input pin states as a binary bitmask (read-only). The least significant bit (LSB) maps to MIO0, with each subsequent bit mapping to higher channel indices.
- `enable_bitmask` (uint, required) — MIO enable states as a binary bitmask. Indicates which channels are enabled for MIO operation. The least significant bit (LSB) maps to MIO0, with each subsequent bit mapping to higher channel indices.
- `channels` (list of MioChannel, required) — Per-channel detailed information

## Errors

### 500 Internal Server Error

Unexpected response format from sensor

- `any`

## Types

### MioChannel

- `aliases` (list of string, required) — Alternative names for the channel
- `input` (boolean, required) — Current input state of the channel (read-only).
- `enable` (boolean, required) — Whether the channel is enabled for MIO operation.
- `config` (enum, required) — Current channel configuration mode. 'OTHER' indicates the channel is not available for MIO operation. If enable is not set and config is OTHER, the channel is used by another service.
  - Allowed values: `INPUT`, `OTHER`

## Examples

**Response**

```json
{
  "input_bitmask": 1,
  "enable_bitmask": 3,
  "channels": [
    {
      "aliases": [
        "MIO0",
        "SYNC_PULSE_IN"
      ],
      "input": false,
      "enable": true,
      "config": "OTHER"
    },
    {
      "aliases": [
        "MIO1",
        "MULTIPURPOSE_IO"
      ],
      "input": true,
      "enable": true,
      "config": "INPUT"
    }
  ]
}
```

**SDK Code**

```python
import requests

url = "http://os-992244000006.local/api/v1/sensor/mio"

response = requests.get(url)

print(response.json())
```

```javascript
const url = 'http://os-992244000006.local/api/v1/sensor/mio';
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
	url := "http://os-992244000006.local/api/v1/sensor/mio"
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
url = URI("http://os-992244000006.local/api/v1/sensor/mio")
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
HttpResponse<String> response = Unirest.get("http://os-992244000006.local/api/v1/sensor/mio")
  .asString();
```

```php
<?php
require_once('vendor/autoload.php');

$client = new \GuzzleHttp\Client();

$response = $client->request('GET', 'http://os-992244000006.local/api/v1/sensor/mio');

echo $response->getBody();
```

```csharp
using RestSharp;

var client = new RestClient("http://os-992244000006.local/api/v1/sensor/mio");
var request = new RestRequest(Method.GET);
IRestResponse response = client.Execute(request);
```

```swift
import Foundation

let request = NSMutableURLRequest(url: NSURL(string: "http://os-992244000006.local/api/v1/sensor/mio")! as URL,