# Get custom profile configuration

GET http://os-992244000006.local/api/v1/sensor/custom_profile

Returns the `udp_profile_lidar_custom` configuration as a `CustomProfile`
object from the requested config source. Defaults to `staged`. Returns
`null` when no custom profile is configured.


Reference: https://docs.ouster.com/sensor-docs/firmware/api-reference/ouster-http-api/sensor-metadata/get-custom-profile

## Request

### Query parameters

- `source` (enum, optional, default: staged) — Config source to read from.
  - Allowed values: `staged`, `active`

## Response

### 200

Custom profile configuration, or null when none

- `n_words` (integer, required) — Number of 32-bit output words in the custom profile.
- `fields` (list of CustomProfileField, required) — Placed fields within the custom profile word layout.

## Errors

### 400 Bad Request Error

Invalid `source` query parameter

- `any`

### 500 Internal Server Error

Failed to read custom profile from keeper

- `any`

## Types

### CustomProfileField

A single placed field in a custom profile. Allowed `view_id` and `variant_id` values are firmware-build-specific; use `GET /sensor/custom_profile/fields` for the authoritative list. `return_index` is required for multi-return data views.

- `view_id` (string, required)
- `offset` (integer, required) — Bit offset from the start of word 0.
- `variant_id` (string, optional)
- `return_index` (integer, optional)

## Examples

**Response**

```json
{
  "n_words": 2,
  "fields": [
    {
      "view_id": "range",
      "offset": 0,
      "variant_id": "eight_mm",
      "return_index": 0
    },
    {
      "view_id": "reflectivity",
      "offset": 16,
      "return_index": 0
    },
    {
      "view_id": "near_infrared",
      "offset": 32,
      "variant_id": "nir"
    }
  ]
}
```

**SDK Code**

```python
import requests

url = "http://os-992244000006.local/api/v1/sensor/custom_profile"

response = requests.get(url)

print(response.json())
```

```javascript
const url = 'http://os-992244000006.local/api/v1/sensor/custom_profile';
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
	url := "http://os-992244000006.local/api/v1/sensor/custom_profile"
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
url = URI("http://os-992244000006.local/api/v1/sensor/custom_profile")
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
HttpResponse<String> response = Unirest.get("http://os-992244000006.local/api/v1/sensor/custom_profile")
  .asString();
```

```php
<?php
require_once('vendor/autoload.php');

$client = new \GuzzleHttp\Client();

$response = $client->request('GET', 'http://os-992244000006.local/api/v1/sensor/custom_profile');

echo $response->getBody();
```

```csharp
using RestSharp;

var client = new RestClient("http://os-992244000006.local/api/v1/sensor/custom_profile");
var request = new RestRequest(Method.GET);
IRestResponse response = client.Execute(request);
```

```swift
import Foundation

let request = NSMutableURLRequest(url: NSURL(string: "http://os-992244000006.local/api/v1/sensor/custom_profile")! as URL,