# Get factory profile layout template

GET http://os-992244000006.local/api/v1/sensor/custom_profile/template/{udp_profile_lidar}

Returns the factory pixel assembler field layout for a built-in UDP lidar
profile via keeper command `get_active_asm_config {profile}`. Use this as a
starting template when authoring a custom profile. `CUSTOM` is not a valid
template. Returns a `CustomProfile` object or `null` when unavailable.
In mock/recovery mode returns `null`.

Reference: https://docs.ouster.com/sensor-docs/firmware/api-reference/ouster-http-api/sensor-metadata/get-custom-profile-template

## Request

### Path parameters

- `udp_profile_lidar` (string, required) — Built-in UDP lidar profile name (alphanumeric and underscore only), e.g. `RNG15_RFL8_NIR8`.

## Response

### 200

Factory layout template for the requested profile, or null when unavailable

- `n_words` (integer, required) — Number of 32-bit output words in the custom profile.
- `fields` (list of CustomProfileField, required) — Placed fields within the custom profile word layout.

## Errors

### 400 Bad Request Error

Invalid or unsupported `udp_profile_lidar` path parameter

- `any`

### 500 Internal Server Error

Failed to read profile template from keeper

- `any`

## Types

### CustomProfileField

A single placed field in a custom profile. Allowed `view_id` and `variant_id` values are firmware-build-specific; use `GET /sensor/custom_profile/fields` for the authoritative list. `return_index` is required for multi-return data views.

- `view_id` (string, required)
- `offset` (integer, required) — Bit offset from the start of word 0.
- `variant_id` (string, optional)
- `return_index` (integer, optional)

## Examples

**Response**

```json
{
  "n_words": 2,
  "fields": [
    {
      "view_id": "range",
      "offset": 0,
      "variant_id": "eight_mm",
      "return_index": 0
    },
    {
      "view_id": "reflectivity",
      "offset": 16,
      "return_index": 0
    },
    {
      "view_id": "near_infrared",
      "offset": 32,
      "variant_id": "nir"
    }
  ]
}
```

**SDK Code**

```python
import requests

url = "http://os-992244000006.local/api/v1/sensor/custom_profile/template/udp_profile_lidar"

response = requests.get(url)

print(response.json())
```

```javascript
const url = 'http://os-992244000006.local/api/v1/sensor/custom_profile/template/udp_profile_lidar';
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
	url := "http://os-992244000006.local/api/v1/sensor/custom_profile/template/udp_profile_lidar"
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
url = URI("http://os-992244000006.local/api/v1/sensor/custom_profile/template/udp_profile_lidar")
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
HttpResponse<String> response = Unirest.get("http://os-992244000006.local/api/v1/sensor/custom_profile/template/udp_profile_lidar")
  .asString();
```

```php
<?php
require_once('vendor/autoload.php');

$client = new \GuzzleHttp\Client();

$response = $client->request('GET', 'http://os-992244000006.local/api/v1/sensor/custom_profile/template/udp_profile_lidar');

echo $response->getBody();
```

```csharp
using RestSharp;

var client = new RestClient("http://os-992244000006.local/api/v1/sensor/custom_profile/template/udp_profile_lidar");
var request = new RestRequest(Method.GET);
IRestResponse response = client.Execute(request);
```

```swift
import Foundation

let request = NSMutableURLRequest(url: NSURL(string: "http://os-992244000006.local/api/v1/sensor/custom_profile/template/udp_profile_lidar")! as URL,