# Secure Mode

> Require authentication before sensor configuration, with relaxed or strict reset policies.

> **Note**
>
> Secure Mode is available in firmware v4.0 or later only.

Use this guide to configure secure mode on the sensor.

By default, the sensor can be configured without authentication. With Secure Mode turned on the sensor can only be configured after successful authentication.

## Secure Mode Terminology

**Reset Policy**
Can be set to either `relaxed` or `strict`. Setting the Reset Policy to `relaxed` is meant to be used for development purposes. In production setting the Reset Policy to `strict` is recommended.

**RBAC Roles**
Secure Mode includes three roles: Guest, Operator, Admin. The Guest role can read all parameters of the sensor configuration. The Operator role can configure all parameters of the sensor configuration except uploading firmware updates and disabling Secure Mode. The Admin role can do everything the Operator role can do and update the firmware of the sensor and disable Secure Mode.

**HTTP redirect**
When `true` (default), HTTP :80 redirects to HTTPS while Secure Mode is active. When `false`, HTTP and HTTPS are both served so existing API clients are not broken.

**Generate Passwords**
The sensor is equipped with a True Random Number Generator (TRNG), which can be used to generate strong random passwords.

## Enabling Secure Mode

Secure Mode can be enabled using the web interface or the HTTP API.

### Web Interface

1. Open the sensor web interface.
2. Go to **Configuration > System**.
3. In **Security (Secure Mode)**, click on **Enable Secure Mode**.
4. On the first page of the **Enable Secure Mode** wizard, choose a Reset Policy and click on **Next**.
5. On the second page of the **Enable Secure Mode** wizard, choose your passwords or let the sensor generate passwords for the Admin and Operators roles and then click the **Enable Secure Mode** button.
6. On the third and last page of the **Enable Secure Mode** wizard, the sensor will provide the Admin and Operator passwords - Save these passwords now!

### HTTP API

**Command**

```shell
curl https://os-992623000385.ouster.internal/api/v1/auth/secure-mode/enable \
  --request POST \
  --header 'Content-Type: application/json' \
  --data '{
  "reset_policy": "relaxed",
  "http_redirect": true,
  "generate": true,
  "include_operator": true,
  "passwords": {
    "admin": "",
    "operator": ""
  }
}'
```

**Response**

```json
{
  "status": "enabled",
  "generated_passwords": {
    "propertyName*": "string"
  }
}
```

## Determine Secure Mode State

When Secure Mode is enabled on the sensor, the web interface displays a **Log in** button on the top right.

The current state of Secure Mode on the sensor can also be queried through the HTTP API.

### HTTP API

**Command**

```shell
curl https://os-992623000385.ouster.internal/api/v1/auth/secure-mode/status
```

**Response**

```json
{
  "enabled": true,
  "provisioned": true,
  "https_provisioned": true,
  "reset_policy": "relaxed",
  "http_redirect": true,
  "roles_set": [
    "admin"
  ]
}
```

## Rotate Passwords

The `admin` role can rotate the passwords of the `operator` and `admin` roles.

### Web Interface

1. Open the sensor web interface.
2. Go to **Configuration > System**.
3. In **Security (Secure Mode)** under **Rotate password**, choose a Role and click on button `Rotate password`.

### HTTP API

**Command**

```shell
curl https://os-992623000385.ouster.internal/api/v1/auth/passwords/admin \
  --request PUT \
  --header 'Content-Type: application/json' \
  --data '{
  "password": "",
  "generate": true
}'
```

**Response**

```json
{
  "role": "admin",
  "password": "string"
}
```

## Disable Secure Mode

> **Note**
>
> If **Reset Policy** is set to `relaxed`, Secure Mode can be disabled by calling the HTTP API endpoint without authentication. To prevent this behavior, set the **Reset Policy** to `strict`.

Secure Mode can be disabled through the sensor's web interface and HTTP API. Disabling Secure Mode requires authenticating with the `admin` role.

### Web Interface

1. Open the sensor web interface and authenticate as `admin`.
2. Go to **Configuration > System**.
3. In **Security (Secure Mode)**, click on button `Disable Secure Mode`.

### HTTP API

**Command**

```shell
curl https://os-992623000385.ouster.internal/api/v1/auth/secure-mode/disable \
  --request POST
```

**Response**

```json
{
  "status": "disabled"
}
```