# Frame Start Control

> Rotate the lidar frame start azimuth to control where each scan frame begins.

> **Note**
>
> Supported in firmware v3.2 or later.

Configurable start-of-frame control is available through `lidar_frame_azimuth_offset`. This parameter rotates the lidar frame in millidegrees, shifting the azimuth at which each frame starts.

For example, setting `lidar_frame_azimuth_offset` to `90000` rotates the lidar frame by 90 degrees. Other angular configuration parameters, such as `azimuth_window` and `phase_lock_offset`, are applied relative to this offset.

Set the offset with [`POST /api/v1/sensor/config`](/sensor-docs/firmware/api-reference#sensor-configuration):

```shell
curl -X POST http://os-991234567890.local/api/v1/sensor/config \
  -H 'Content-Type: application/json' \
  --data '{"lidar_frame_azimuth_offset": 90000}'
```