# Bloom Reduction Optimization

> Tune the tradeoff between suppressing retroreflector blooming artifacts and preserving nearby detections.

> **Note**
>
> Supported in firmware v3.2 or later.

The `bloom_reduction_optimization` configuration parameter is used for scenes with strong retroreflectors. Use it to tune the tradeoff between suppressing blooming artifacts and preserving true detections near bright objects.

Valid values are:

* `BALANCED` (default) - balances false positives and false negatives.
* `MINIMIZE_FALSE_POSITIVES` - more aggressively suppresses blooming artifacts near retroreflectors.

Set the parameter with [`POST /api/v1/sensor/config`](/sensor-docs/firmware/api-reference#sensor-configuration):

```shell
curl -X POST http://os-991234567890.local/api/v1/sensor/config \
  -H 'Content-Type: application/json' \
  --data '{"bloom_reduction_optimization": "MINIMIZE_FALSE_POSITIVES"}'
```