# Overview of the firmware

GET http://os-992244000006.local/api/v1/system/firmware

Provides update progress and firmware version

Reference: https://docs.ouster.com/sensor-docs/firmware/api-reference/ouster-http-api/system/get-firmware

## Response

### 200

Running firmware image name and version

- `commit_pending` (boolean, optional)
- `update_status` (enum, optional) — Current status of the firmware update. A normal update transitions from PENDING to either COMPLETE or FAILED. PENDING_RECOVERY requires the system to be rebooted before attempting an update.
  - Allowed values: `COMPLETE`, `FAILED`, `PENDING`, `PENDING_RECOVERY`
- `fw` (string, optional)
- `semver` (string, optional)

## Examples

**Response**

```json
{
  "commit_pending": false,
  "update_status": "COMPLETE",
  "fw": "ousteros-image-prod-bootes-v3.0.0+0123456789",
  "semver": "3.0.0+0123456789"
}
```

**SDK Code**

```python
import requests

url = "http://os-992244000006.local/api/v1/system/firmware"

response = requests.get(url)

print(response.json())
```

```javascript
const url = 'http://os-992244000006.local/api/v1/system/firmware';
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
	url := "http://os-992244000006.local/api/v1/system/firmware"
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
url = URI("http://os-992244000006.local/api/v1/system/firmware")
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
HttpResponse<String> response = Unirest.get("http://os-992244000006.local/api/v1/system/firmware")
  .asString();
```

```php
<?php
require_once('vendor/autoload.php');

$client = new \GuzzleHttp\Client();

$response = $client->request('GET', 'http://os-992244000006.local/api/v1/system/firmware');

echo $response->getBody();
```

```csharp
using RestSharp;

var client = new RestClient("http://os-992244000006.local/api/v1/system/firmware");
var request = new RestRequest(Method.GET);
IRestResponse response = client.Execute(request);
```

```swift
import Foundation

let request = NSMutableURLRequest(url: NSURL(string: "http://os-992244000006.local/api/v1/system/firmware")! as URL,