# Enable Secure Mode and provision passwords

POST http://os-992244000006.local/api/v1/auth/secure-mode/enable
Content-Type: application/json

Reference: https://docs.ouster.com/sensor-docs/firmware/api-reference/ouster-http-api/secure-mode/post-secure-mode-enable

## Request

### Body (application/json)

This endpoint expects a SecureModeEnableRequest.

- `reset_policy` (enum, required)
  - Allowed values: `relaxed`, `strict`
- `http_redirect` (boolean, optional, default: true) — When true (default), HTTP :80 redirects to HTTPS while Secure Mode is active. When false, HTTP and HTTPS are both served so existing API clients are not broken.
- `generate` (boolean, optional) — Generate random passwords instead of using passwords below. Cannot be used together with a passwords object.
- `include_operator` (boolean, optional, default: true) — When generate is true, also generate an operator password
- `passwords` (SecureModeEnableRequestPasswords, optional) — Required when generate is false; must not be supplied when generate is true. Passwords must be at least 13 characters and include at least 3 of 4 character types (lowercase, uppercase, digits, special characters).

## Response

### 200

Enabled

- `status` (enum, required)
  - Allowed values: `enabled`
- `generated_passwords` (map from string to string, optional, nullable) — Present when generate was true; returned once in plaintext

## Errors

### 400 Bad Request Error

Invalid request or missing admin password

- `title` (string, optional) — Error title
- `description` (string, optional) — Error description

### 401 Unauthorized Error

Re-provisioning requires an admin session

- `title` (string, optional) — Error title
- `description` (string, optional) — Error description

### 403 Forbidden Error

Request must be sent over HTTPS

- `title` (string, optional) — Error title
- `description` (string, optional) — Error description

### 409 Conflict Error

Secure Mode is already enabled and provisioned

- `title` (string, optional) — Error title
- `description` (string, optional) — Error description

## Types

### SecureModeEnableRequestPasswords

Required when generate is false; must not be supplied when generate is true. Passwords must be at least 13 characters and include at least 3 of 4 character types (lowercase, uppercase, digits, special characters).

- `admin` (string, optional)
- `operator` (string, optional)

## Examples

**Request**

```json
{
  "reset_policy": "relaxed"
}
```

**Response**

```json
{
  "status": "enabled",
  "generated_passwords": {}
}
```

**SDK Code**

```python
import requests

url = "http://os-992244000006.local/api/v1/auth/secure-mode/enable"

payload = { "reset_policy": "relaxed" }
headers = {"Content-Type": "application/json"}

response = requests.post(url, json=payload, headers=headers)

print(response.json())
```

```javascript
const url = 'http://os-992244000006.local/api/v1/auth/secure-mode/enable';
const options = {
  method: 'POST',
  headers: {'Content-Type': 'application/json'},
  body: '{"reset_policy":"relaxed"}'
};
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
	"strings"
	"net/http"
	"io"
)

func main() {

	url := "http://os-992244000006.local/api/v1/auth/secure-mode/enable"

	payload := strings.NewReader("{\n  \"reset_policy\": \"relaxed\"\n}")

	req, _ := http.NewRequest("POST", url, payload)

	req.Header.Add("Content-Type", "application/json")
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
url = URI("http://os-992244000006.local/api/v1/auth/secure-mode/enable")

http = Net::HTTP.new(url.host, url.port)

request = Net::HTTP::Post.new(url)
request["Content-Type"] = 'application/json'
request.body = "{\n  \"reset_policy\": \"relaxed\"\n}"

response = http.request(request)
puts response.read_body
```

```java
import com.mashape.unirest.http.HttpResponse;
import com.mashape.unirest.http.Unirest;

HttpResponse<String> response = Unirest.post("http://os-992244000006.local/api/v1/auth/secure-mode/enable")
  .header("Content-Type", "application/json")
  .body("{\n  \"reset_policy\": \"relaxed\"\n}")
  .asString();
```

```php
<?php
require_once('vendor/autoload.php');

$client = new \GuzzleHttp\Client();

$response = $client->request('POST', 'http://os-992244000006.local/api/v1/auth/secure-mode/enable', [
  'body' => '{
  "reset_policy": "relaxed"
}',
  'headers' => [
    'Content-Type' => 'application/json',
  ],
]);

echo $response->getBody();
```

```csharp
using RestSharp;

var client = new RestClient("http://os-992244000006.local/api/v1/auth/secure-mode/enable");
var request = new RestRequest(Method.POST);
request.AddHeader("Content-Type", "application/json");
request.AddParameter("application/json", "{\n  \"reset_policy\": \"relaxed\"\n}", ParameterType.RequestBody);
IRestResponse response = client.Execute(request);
```

```swift
import Foundation

let headers = ["Content-Type": "application/json"]
let parameters = ["reset_policy": "relaxed"] as [String : Any]

let postData = JSONSerialization.data(withJSONObject: parameters, options: [])

let request = NSMutableURLRequest(url: NSURL(string: "http://os-992244000006.local/api/v1/auth/secure-mode/enable")! as URL,
                                        cachePolicy: .useProtocolCachePolicy,
                                    timeoutInterval: 10.0)
request.httpMethod = "POST"
request.allHTTPHeaderFields = headers
request.httpBody = postData as Data