# Get the telemetry information

GET http://os-992244000006.local/api/v1/sensor/telemetry

Get the sensor telemetry information

Reference: https://docs.ouster.com/sensor-docs/firmware/api-reference/ouster-http-api/alerts-diagnostics-and-telemetry/get-telemetry

## Response

### 200

Valid telemetry query result

- `timestamp_ns` (uint64, optional) — Time at which the information was collected
- `phase_lock_status` (enum, optional) — Motor phase lock status. `INTERNAL` when the internal time reference is configured (`TIME_FROM_INTERNAL_OSC`) and motor is operating nominally. `LOCKED` when external time sync is configured (`TIME_FROM_SYNC_PULSE_IN`, `TIME_FROM_PTP_1588`) and motor phase lock is acquired; sync pulse input lock loss is reflected when applicable. `LOST` when motor phase lock is not currently held, including standby, spin-up, and external sync source loss. PTP time synchronization lock state is not reflected in this field.
  - Allowed values: `INTERNAL`, `LOCKED`, `LOST`
- `input_voltage_mv` (integer, optional) — Reports system input-voltage in millvolts
- `internal_temperature_deg_c` (integer, optional) — Reports system temperature in degrees C Only available on Rev 06 and above sensors.
- `input_current_ma` (integer, optional) — System input-current in milliamps

## Examples

**Response**

```json
{
  "timestamp_ns": 1682547890123456800,
  "phase_lock_status": "LOCKED",
  "input_voltage_mv": 12000,
  "internal_temperature_deg_c": 45,
  "input_current_ma": 850
}
```

**SDK Code**

```python
import requests

url = "http://os-992244000006.local/api/v1/sensor/telemetry"

response = requests.get(url)

print(response.json())
```

```javascript
const url = 'http://os-992244000006.local/api/v1/sensor/telemetry';
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
	url := "http://os-992244000006.local/api/v1/sensor/telemetry"
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
url = URI("http://os-992244000006.local/api/v1/sensor/telemetry")
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
HttpResponse<String> response = Unirest.get("http://os-992244000006.local/api/v1/sensor/telemetry")
  .asString();
```

```php
<?php
require_once('vendor/autoload.php');

$client = new \GuzzleHttp\Client();

$response = $client->request('GET', 'http://os-992244000006.local/api/v1/sensor/telemetry');

echo $response->getBody();
```

```csharp
using RestSharp;

var client = new RestClient("http://os-992244000006.local/api/v1/sensor/telemetry");
var request = new RestRequest(Method.GET);
IRestResponse response = client.Execute(request);
```

```swift
import Foundation

let request = NSMutableURLRequest(url: NSURL(string: "http://os-992244000006.local/api/v1/sensor/telemetry")! as URL,