# Standby Operating Mode

> Put the sensor into a low-power state while keeping it responsive to commands.

Standby Operating Mode that can be useful for power, battery, or thermal-conscious applications of the sensor.

The `operating_mode` config parameter defaults to `NORMAL`. Set it to `STANDBY` and reinitialize to enter Standby mode.

#### Expected Sensor Behavior

Standby power draw: 5 W. The motor does not spin and the laser is off, but the sensor remains on and responsive to commands. Status reports as `STANDBY`.

#### Standby Operating Mode Examples

Use the [sensor configuration endpoint](/sensor-docs/firmware/api-reference#sensor-configuration) to set `operating_mode`. A successful configuration request reinitializes the sensor automatically.

Set the sensor to Standby mode and keep it in Standby mode after the next power cycle:

```shell
curl -X POST "http://os-991900123456.local/api/v1/sensor/config?target=persisted" \
  -H "Content-Type: application/json" \
  --data '{"operating_mode": "STANDBY"}'
```

Set the sensor to Standby mode temporarily, without changing the persisted startup configuration:

```shell
curl -X POST "http://os-991900123456.local/api/v1/sensor/config?target=active" \
  -H "Content-Type: application/json" \
  --data '{"operating_mode": "STANDBY"}'
```

Return the sensor to Running mode and save that configuration:

```shell
curl -X POST "http://os-991900123456.local/api/v1/sensor/config?target=persisted" \
  -H "Content-Type: application/json" \
  --data '{"operating_mode": "NORMAL"}'
```