# Sensor Telemetry

> Query live sensor health data including temperature, voltage, and phase lock status.

Sensor telemetry reports live system state—temperature, voltage, and related parameters—for diagnostics and preventive action. Query it with the [telemetry endpoint](/sensor-docs/firmware/api-reference#alerts-and-diagnostics):

```json
{
  "input_current_ma": 644,
  "input_voltage_mv": 23624,
  "internal_temperature_deg_c": 48,
  "phase_lock_status": "DISABLED",
  "timestamp_ns": 2093396806056
}
```

| Fields               | Notes                                                                                                           |
| -------------------- | --------------------------------------------------------------------------------------------------------------- |
| Timestamp            | Timestamp from the FPGA measured in `ns` (Nanoseconds)                                                          |
| Lidar Input Voltage  | Input voltage `mv` (Millivolt) that is provided to the sensor                                                   |
| Lidar Input Current  | Input current `ma` (Milliamp) that is provided to the sensor                                                    |
| Internal Temperature | Internal base board temperature `ºC` (Degree Celsius).                                                          |
| Phase Lock Status    | Different codes to specify phase lock status and issues related to phase locking (`LOCKED`, `LOST`, `DISABLED`) |

> **Note**
>
> * Sensor telemetry will be available on all sensor revisions but internal temperature value can only be measured with **Rev 06** and above sensors. - **Phase lock** output will not indicate loss of lock if the PTP source is lost.