# Get render time estimate for zone set

GET http://os-992244000006.local/api/v1/zone_monitor/{zone_set}/render_estimate

Returns an estimate of the time required to render STL files without corresponding ZRBs. Zones that have ZRBs already rendered are not counted, even if config have been changes made that will invalidate them.

Reference: https://docs.ouster.com/sensor-docs/firmware/api-reference/ouster-http-api/zone-monitor/get-render-time-estimate-for-zone-set

## Request

### Path parameters

- `zone_set` (enum, required) — Zone set identifier. Valid values are 'active' or 'staged'. The 'pending' set is a transient state and should not be used.
  - Allowed values: `active`, `staged`

## Response

### 200

Render time estimate

- `estimate_ms` (integer, required) — Estimated render time in milliseconds
- `total_triangles` (integer, required) — Total number of triangles across zones needing rendering
- `zone_count` (integer, required) — Number of zones that need rendering

## Examples

**Response**

```json
{
  "estimate_ms": 1250,
  "total_triangles": 45230,
  "zone_count": 7
}
```

**SDK Code**

```python
import requests

url = "http://os-992244000006.local/api/v1/zone_monitor/active/render_estimate"

response = requests.get(url)

print(response.json())
```

```javascript
const url = 'http://os-992244000006.local/api/v1/zone_monitor/active/render_estimate';
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
	url := "http://os-992244000006.local/api/v1/zone_monitor/active/render_estimate"
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
url = URI("http://os-992244000006.local/api/v1/zone_monitor/active/render_estimate")
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
HttpResponse<String> response = Unirest.get("http://os-992244000006.local/api/v1/zone_monitor/active/render_estimate")
  .asString();
```

```php
<?php
require_once('vendor/autoload.php');

$client = new \GuzzleHttp\Client();

$response = $client->request('GET', 'http://os-992244000006.local/api/v1/zone_monitor/active/render_estimate');

echo $response->getBody();
```

```csharp
using RestSharp;

var client = new RestClient("http://os-992244000006.local/api/v1/zone_monitor/active/render_estimate");
var request = new RestRequest(Method.GET);
IRestResponse response = client.Execute(request);
```

```swift
import Foundation

let request = NSMutableURLRequest(url: NSURL(string: "http://os-992244000006.local/api/v1/zone_monitor/active/render_estimate")! as URL,