> For clean Markdown of any page, append .md to the page URL. > For a complete documentation index, see https://docs.ouster.com/sensor-docs/firmware/3.2/api-reference/ouster-http-api/system/put-network-i-pv-4-override/llms.txt. > For AI client integration (Claude Code, Cursor, etc.), connect to the MCP server at https://docs.ouster.com/_mcp/server. # Override a static IP address PUT http://os-992244000006.local/api/v1/system/network/ipv4/override Content-Type: application/json Override the default dynamic behavior and set a static IP address and optional gateway. __Note:__ The sensor will reset the network configuration after a short sub second delay (to allow for the HTTP response to be sent). After this delay the sensor will only be reachable on the newly set IPv4 address. The sensor needs to be reachable either by link-local or dynamic DHCP configuration or by an existing static IP override from the host reconfiguring the sensor. The sensor may be reset back to using DHCP with `DELETE api/v1/sensor/config`. __Warning:__ If an unreachable network address is set, the sensor will not be accessible. Tools such as avahi-browse, dns-sd, or mDNS browser can help with finding a sensor on a network. Static IP override should only be used in special use cases. DHCP configuration is recommended where possible. __Note:__ Sensor can be accessed on the sensor's self-assigned link-local IPv4 or IPv6 addresses, in case the sensor becomes unreachable on the configured network due to a misconfiguration. To discover the self-assigned link-local IPv4 or IPv6 addresses for a sensor one can use a network sniffer (such as wireshark) on the same network segment as the sensor. Reference: https://docs.ouster.com/sensor-docs/firmware/api-reference/ouster-http-api/system/put-network-i-pv-4-override ## Request ### Body (application/json) This endpoint expects a System_putNetworkIPv4Override_Request. - `System_putNetworkIPv4Override_Request` ## Response ### 200 No error ## Types ### IPv4Override Recommended IP address format - `addr` (string, required) - `gateway` (string, optional) ## Examples **Request** ```json { "addr": "192.168.200.2/24" } ``` **Response** ```json {} ``` **SDK Code** ```python import requests url = "http://os-992244000006.local/api/v1/system/network/ipv4/override" payload = { "addr": "192.168.200.2/24" } headers = {"Content-Type": "application/json"} response = requests.put(url, json=payload, headers=headers) print(response.json()) ``` ```javascript const url = 'http://os-992244000006.local/api/v1/system/network/ipv4/override'; const options = { method: 'PUT', headers: {'Content-Type': 'application/json'}, body: '{"addr":"192.168.200.2/24"}' }; try { const response = await fetch(url, options); const data = await response.json(); console.log(data); } catch (error) { console.error(error); } ``` ```go package main import ( "fmt" "strings" "net/http" "io" ) func main() { url := "http://os-992244000006.local/api/v1/system/network/ipv4/override" payload := strings.NewReader("{\n \"addr\": \"192.168.200.2/24\"\n}") req, _ := http.NewRequest("PUT", url, payload) req.Header.Add("Content-Type", "application/json") res, _ := http.DefaultClient.Do(req) defer res.Body.Close() body, _ := io.ReadAll(res.Body) fmt.Println(res) fmt.Println(string(body)) } ``` ```ruby require 'uri' require 'net/http' url = URI("http://os-992244000006.local/api/v1/system/network/ipv4/override") http = Net::HTTP.new(url.host, url.port) request = Net::HTTP::Put.new(url) request["Content-Type"] = 'application/json' request.body = "{\n \"addr\": \"192.168.200.2/24\"\n}" response = http.request(request) puts response.read_body ``` ```java import com.mashape.unirest.http.HttpResponse; import com.mashape.unirest.http.Unirest; HttpResponse response = Unirest.put("http://os-992244000006.local/api/v1/system/network/ipv4/override") .header("Content-Type", "application/json") .body("{\n \"addr\": \"192.168.200.2/24\"\n}") .asString(); ``` ```php request('PUT', 'http://os-992244000006.local/api/v1/system/network/ipv4/override', [ 'body' => '{ "addr": "192.168.200.2/24" }', 'headers' => [ 'Content-Type' => 'application/json', ], ]); echo $response->getBody(); ``` ```csharp using RestSharp; var client = new RestClient("http://os-992244000006.local/api/v1/system/network/ipv4/override"); var request = new RestRequest(Method.PUT); request.AddHeader("Content-Type", "application/json"); request.AddParameter("application/json", "{\n \"addr\": \"192.168.200.2/24\"\n}", ParameterType.RequestBody); IRestResponse response = client.Execute(request); ``` ```swift import Foundation let headers = ["Content-Type": "application/json"] let parameters = ["addr": "192.168.200.2/24"] as [String : Any] let postData = JSONSerialization.data(withJSONObject: parameters, options: []) let request = NSMutableURLRequest(url: NSURL(string: "http://os-992244000006.local/api/v1/system/network/ipv4/override")! as URL, cachePolicy: .useProtocolCachePolicy, timeoutInterval: 10.0) request.httpMethod = "PUT" request.allHTTPHeaderFields = headers request.httpBody = postData as Data let session = URLSession.shared let dataTask = session.dataTask(with: request as URLRequest, completionHandler: { (data, response, error) -> Void in if (error != nil) { print(error as Any) } else { let httpResponse = response as? HTTPURLResponse print(httpResponse) } }) dataTask.resume() ```