> For clean Markdown of any page, append .md to the page URL. > For a complete documentation index, see https://docs.ouster.com/sensor-docs/firmware/3.2/api-reference/ouster-http-api/system/llms.txt. > For AI client integration (Claude Code, Cursor, etc.), connect to the MCP server at https://docs.ouster.com/sensor-docs/_mcp/server. # System ## API Docs - [Restarts the sensor](https://docs.ouster.com/sensor-docs/firmware/3.2/api-reference/ouster-http-api/system/post-restart.md): System - [Overview of the firmware](https://docs.ouster.com/sensor-docs/firmware/3.2/api-reference/ouster-http-api/system/get-firmware.md): System - [Update the firmware](https://docs.ouster.com/sensor-docs/firmware/3.2/api-reference/ouster-http-api/system/post-firmware.md): System - [Get the system network configuration](https://docs.ouster.com/sensor-docs/firmware/3.2/api-reference/ouster-http-api/system/get-network.md): System - [Get the IPv4 network configuration](https://docs.ouster.com/sensor-docs/firmware/3.2/api-reference/ouster-http-api/system/get-network-i-pv-4.md): System - [Get the current IPv4 static IP address override](https://docs.ouster.com/sensor-docs/firmware/3.2/api-reference/ouster-http-api/system/get-network-i-pv-4-override.md): System - [Override a static IP address](https://docs.ouster.com/sensor-docs/firmware/3.2/api-reference/ouster-http-api/system/put-network-i-pv-4-override.md): System - [Delete the static IP override](https://docs.ouster.com/sensor-docs/firmware/3.2/api-reference/ouster-http-api/system/delete-network-i-pv-4-override.md): System - [Get T1 ethernet speed override](https://docs.ouster.com/sensor-docs/firmware/3.2/api-reference/ouster-http-api/system/get-network-speed-override.md): System - [Set T1 ethernet speed override](https://docs.ouster.com/sensor-docs/firmware/3.2/api-reference/ouster-http-api/system/put-network-speed-override.md): System - [Reset the T1 ethernet speed override](https://docs.ouster.com/sensor-docs/firmware/3.2/api-reference/ouster-http-api/system/delete-network-speed-override.md): System ## OpenAPI Specification - [OpenAPI JSON](https://docs.ouster.com/sensor-docs/openapi.json): raw OpenAPI 3.1 specification for this API, JSON format - [OpenAPI YAML](https://docs.ouster.com/sensor-docs/openapi.yaml): raw OpenAPI 3.1 specification for this API, YAML format