# Get a single configuration parameter

GET http://os-992244000006.local/api/v1/sensor/config/{param}

Get a single sensor configuration parameter

Reference: https://docs.ouster.com/sensor-docs/firmware/api-reference/ouster-http-api/sensor-metadata/get-config-single

## Request

### Path parameters

- `param` (enum, required)
  - Allowed values: `accel_fsr`, `azimuth_window`, `columns_per_packet`, `gyro_fsr`, `imu_packets_per_frame`, `lidar_frame_azimuth_offset`, `lidar_mode`, `min_range_threshold_cm`, `multipurpose_io_mode`, `nmea_baud_rate`, `nmea_ignore_valid_char`, `nmea_in_polarity`, `nmea_leap_seconds`, `operating_mode`, `phase_lock_enable`, `phase_lock_offset`, `return_order`, `signal_multiplier`, `sync_pulse_in_polarity`, `sync_pulse_out_angle`, `sync_pulse_out_frequency`, `sync_pulse_out_polarity`, `sync_pulse_out_pulse_width`, `timestamp_mode`, `udp_dest`, `udp_port_imu`, `udp_port_lidar`, `udp_multicast_ttl`, `udp_dest_zm`, `udp_port_zm`, `udp_multicast_ttl_zm`, `header_type`, `udp_profile_imu`, `udp_profile_lidar`, `manufacturing_calibration/reflectivity_version`

### Query parameters

- `source` (enum, optional, default: active) — Specifies which configuration source to return: * `active` (default): Returns the currently running configuration * `staged`: Returns the staged configuration (not yet active) * `default`: Returns the factory default configuration values * `persisted`: Returns the configuration read from non-volatile memory
  - Allowed values: `active`, `staged`, `default`, `persisted`

## Response

### 200

The value of a single sensor parameter

- `any`

## Examples

**Response**

```json
"\"RUNNING\""
```

**SDK Code**

```python Sensor Metadata_getConfigSingle_example
import requests

url = "http://os-992244000006.local/api/v1/sensor/config/accel_fsr"

response = requests.get(url)

print(response.json())
```

```javascript Sensor Metadata_getConfigSingle_example
const url = 'http://os-992244000006.local/api/v1/sensor/config/accel_fsr';
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
```go Sensor Metadata_getConfigSingle_example
package main

import (
	"fmt"
	"net/http"
	"io"
)

func main() {

	url := "http://os-992244000006.local/api/v1/sensor/config/accel_fsr"
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
```ruby Sensor Metadata_getConfigSingle_example
require 'uri'
require 'net/http'

url = URI("http://os-992244000006.local/api/v1/sensor/config/accel_fsr")

http = Net::HTTP.new(url.host, url.port)

request = Net::HTTP::Get.new(url)

response = http.request(request)
puts response.read_body
```

```java Sensor Metadata_getConfigSingle_example
import com.mashape.unirest.http.HttpResponse;
import com.mashape.unirest.http.Unirest;

HttpResponse<String> response = Unirest.get("http://os-992244000006.local/api/v1/sensor/config/accel_fsr")
  .asString();
```

```php Sensor Metadata_getConfigSingle_example
<?php
require_once('vendor/autoload.php');

$client = new \GuzzleHttp\Client();

$response = $client->request('GET', 'http://os-992244000006.local/api/v1/sensor/config/accel_fsr');

echo $response->getBody();
```

```csharp Sensor Metadata_getConfigSingle_example
using RestSharp;

var client = new RestClient("http://os-992244000006.local/api/v1/sensor/config/accel_fsr");
var request = new RestRequest(Method.GET);
IRestResponse response = client.Execute(request);
```

```swift Sensor Metadata_getConfigSingle_example
import Foundation

let request = NSMutableURLRequest(url: NSURL(string: "http://os-992244000006.local/api/v1/sensor/config/accel_fsr")! as URL,