> For clean Markdown of any page, append .md to the page URL.
> For a complete documentation index, see https://docs.ouster.com/sensor-docs/llms.txt.
> For AI client integration (Claude Code, Cursor, etc.), connect to the MCP server at https://docs.ouster.com/sensor-docs/_mcp/server.

# Get the telemetry information

GET http://os-992244000006.local/api/v1/sensor/telemetry

Get the sensor telemetry information

Reference: https://docs.ouster.com/sensor-docs/firmware/api-reference/ouster-http-api/alerts-diagnostics-and-telemetry/get-telemetry

## Response

### 200

Valid telemetry query result

- `timestamp_ns` (uint64, optional) — Time at which the information was collected
- `phase_lock_status` (enum, optional) — The current phase-lock status will not indicate loss of lock if the time synchronization is lost.
  - Allowed values: `LOCKED`, `LOST`, `DISABLED`
- `input_voltage_mv` (integer, optional) — Reports system input-voltage in millvolts
- `internal_temperature_deg_c` (integer, optional) — Reports system temperature in degrees C Only available on Rev 06 and above sensors.
- `input_current_ma` (integer, optional) — System input-current in milliamps

## Examples

**Response**

```json
{
  "timestamp_ns": 1682547890123456800,
  "phase_lock_status": "LOCKED",
  "input_voltage_mv": 12000,
  "internal_temperature_deg_c": 45,
  "input_current_ma": 850
}
```

**SDK Code**

```python
import requests

url = "http://os-992244000006.local/api/v1/sensor/telemetry"

response = requests.get(url)

print(response.json())
```

```javascript
const url = 'http://os-992244000006.local/api/v1/sensor/telemetry';
const options = {method: 'GET'};

try {
  const response = await fetch(url, options);
  const data = await response.json();
  console.log(data);
} catch (error) {
  console.error(error);
}
```

```go
package main

import (
	"fmt"
	"net/http"
	"io"
)

func main() {

	url := "http://os-992244000006.local/api/v1/sensor/telemetry"

	req, _ := http.NewRequest("GET", url, nil)

	res, _ := http.DefaultClient.Do(req)

	defer res.Body.Close()
	body, _ := io.ReadAll(res.Body)

	fmt.Println(res)
	fmt.Println(string(body))

}
```

```ruby
require 'uri'
require 'net/http'

url = URI("http://os-992244000006.local/api/v1/sensor/telemetry")

http = Net::HTTP.new(url.host, url.port)

request = Net::HTTP::Get.new(url)

response = http.request(request)
puts response.read_body
```

```java
import com.mashape.unirest.http.HttpResponse;
import com.mashape.unirest.http.Unirest;

HttpResponse<String> response = Unirest.get("http://os-992244000006.local/api/v1/sensor/telemetry")
  .asString();
```

```php
<?php
require_once('vendor/autoload.php');

$client = new \GuzzleHttp\Client();

$response = $client->request('GET', 'http://os-992244000006.local/api/v1/sensor/telemetry');

echo $response->getBody();
```

```csharp
using RestSharp;

var client = new RestClient("http://os-992244000006.local/api/v1/sensor/telemetry");
var request = new RestRequest(Method.GET);
IRestResponse response = client.Execute(request);
```

```swift
import Foundation

let request = NSMutableURLRequest(url: NSURL(string: "http://os-992244000006.local/api/v1/sensor/telemetry")! as URL,
                                        cachePolicy: .useProtocolCachePolicy,
                                    timeoutInterval: 10.0)
request.httpMethod = "GET"

let session = URLSession.shared
let dataTask = session.dataTask(with: request as URLRequest, completionHandler: { (data, response, error) -> Void in
  if (error != nil) {
    print(error as Any)
  } else {
    let httpResponse = response as? HTTPURLResponse
    print(httpResponse)
  }
})

dataTask.resume()
```