Module ouster.sdk.util

ouster.sdk.util.extrinsics

Warning

Deprecated since version 0.15.0 resolve_extrinsics is deprecated. Specify the extrinsics file name explicitly when constructing a scan source instead. resolve_extrinsics will be removed in the upcoming release.

Miscellaneous utilities.

fov_vertical(info)[source]
Return type:

float

fov_horizontal(info)[source]
Return type:

float

img_aspect_ratio(info)[source]

Returns 2D image aspect ratio based on sensor FOV angles.

Return type:

float

Uses the order:

img_aspect_ratio = FOV_vertical / FOV_horizontal

quaternion_to_rotation_matrix(q)[source]

Converts Quaternion [w, x, y, z] to Rotation [3x3] matrix.

Return type:

ndarray

rotation_matrix_to_quaternion(R)[source]

Converts a Rotation [3x3] matrix to Quaternion [w, x, y, z].

Return type:

ndarray

position_quaternion_to_transform(p, q)[source]

Converts Quaternion + Pose [7] vector to homogeneous [4x4] matrix.

Return type:

ndarray

resolve_extrinsics(data_path, infos=[], sensor_names=[])[source]

Find the extrinsics for a data_path and metadata sets.

Return type:

List[Optional[Tuple[ndarray, str]]]

Currently looking for extrinsics in:
  • perception extrinsics_parameters.json in the same directory as a .pcap data_path.

  • perception extrinsics_parameters.json in the tar _configuration.tar in the same directory as a .pcap data_path.

  • simulated data extrinsics.json in the data_path directory with the destination frame names base_link

euler_to_rotation_matrix(roll, pitch, yaw)[source]

Convert Euler angles (roll, pitch, yaw) to a 3D rotation matrix.

Parameters:
  • roll – Rotation about the x-axis (rad)

  • pitch – Rotation about the y-axis (rad)

  • yaw – Rotation about the z-axis (rad)

Returns:

3x3 rotation matrix

Return type:

R

xyzrpy_to_matrix(px, py, pz, r, p, y)[source]

A method that takes position + euler angles (rad) and produces an equivalent 4x4 transform.

Parameters:
  • px – position

  • py – position

  • pz – position

  • r – rotation expressed in euler angles (rad)

  • p – rotation expressed in euler angles (rad)

  • y – rotation expressed in euler angles (rad)

Returns:

4x4 transformation matrix

Return type:

R

xyzq_to_matrix(px, py, pz, qx, qy, qz, qw)[source]

A method that takes position + quaternion (rad) and produces an equivalent 4x4 transform.

Parameters:
  • px – position

  • py – position

  • pz – position

  • qx – rotation expressed in a quaternion

  • qy – rotation expressed in a quaternion

  • qz – rotation expressed in a quaternion

  • qw – rotation expressed in a quaternion

Returns:

4x4 transformation matrix

Return type:

R

parse_extrinsics_from_string(extrinsics, degrees=True)[source]

A utility method to parse extrinsics in multiple formats.

Parameters:
  • extrinsics (- A json with containing a per sensor) – a string representing a file or extrinsics in a supported format

  • degrees – whether angles should be parsed as degress (True by default)

  • formats (Acceptale extrinsics) –

  • extrinsics –

  • identity (- identity ; Use this to override any stored extrinsics with) –

  • angles (- X Y Z R P Y ; 'R P Y' represent euler) –

  • ; (- X Y Z QX QY QZ QW) –

  • order (- n1 n2 .. n16 ; 16 floats representing a 2D array in a row-major) –

Returns:

4x4 transformation matrix or a filename

Return type:

R

ouster.sdk.util.forward_slicer

class ForwardSlicer[source]

Bases: object

ForwardSlicer provides slicing methods to slice up a container with step to containers that only support forward slicing

static normalize(key, L)[source]
Return type:

slice

static slice_iter(data_iter, key)[source]

Performs forward slicing on a dataset with step

Parameters: - key: must be a normalized slice key with relation to the used data_iter.

a normalized slice key is one where key.start < key.stop and no non-values

Returns:

an iterator scoped to the input key

Return type:

Iterator

static slice(data_iter, key)[source]

Performs forward slicing on a dataset with step

Parameters: - key: must be a normalized slice key with relation to the used data_iter.

a normalized slice key is one where key.start < key.stop and no non-values

Returns:

a list of items scoped to the input key

Return type:

List

ouster.sdk.util.metadata

Miscellaneous utilites.

resolve_metadata(data_path, meta_path=None)[source]

Look for a metadata file based on the data path if needed.

Convenient to use in CLI tools when –meta param can be omitted in lots of trivial cases when pcap filename has the same prefix as the metadata json filename.

Parameters:
  • data_path (str) – filename location with the data, usually .pcap or .bag that is used to search metadata with the most common prefix file

  • meta_path (Optional[str]) – the pass through metadata path, if set guessing and search for other metadata jsons is skipped

Return type:

Optional[str]

Returns:

metadata json paths guessed with the most common prefix match or passed through from meta_path parameter

resolve_metadata_multi(data_path)[source]

Look for a metadata files based on the pcap path with multi sensors.

Parameters:

data_path (str) – filename location with the data, usually .pcap or .bag

Return type:

List[str]

Returns:

list of metadata json paths guessed with the most common prefix match

ouster.sdk.util.parsing

R/W implementation of packet parsing.

Doesn’t rely on custom C++ extensions (just numpy). Provides writable view of packet data for testing and development.

default_scan_fields(profile, raw_headers=False)[source]

Get the default fields populated on scans for a profile.

Convenient helper function if you want to tweak which fields are parsed into a LidarScan without listing out the defaults yourself.

Parameters:
  • profile (UDPProfileLidar) – The lidar profile

  • raw_headers (bool) – Include RAW_HEADERS field

Return type:

List[FieldType]

Returns:

A field configuration that can be passed to client.Scans. or None for custom added UDPProfileLidar

tohex(data)[source]

Makes a hex string for debug print outs of buffers.

Selects the biggest devisor of np.uint32, np.uint16 or np.uint8 for making a hex output of the provided data. (clunky but usefull for debugging)

Return type:

str

scan_to_packets(ls, info)[source]

Converts LidarScan to a lidar_packet buffers

Parameters:
  • ls (LidarScan) – LidarScan; if LidarScan has RAW_HEADERS field, packet headers are recreated to how they were in the original packets

  • info (SensorInfo) – metadata of the ls scan

Return type:

List[LidarPacket]

Returns:

A set of lidar packets that will produce the same LidarScan if passed through the ScanBatcher again (less fields data)

terminator_packet(info, last_packet)[source]

Makes a next after the last lidar packet buffer that finishes LidarScan.

Main mechanism is to set the next frame_id (frame_id + 1) in uint16 format of the lidar packet with some arbitrary data (filled with 0xfe).

Such a next after the last lidar packet is needed for the ScanBatcher to correctly finish the scan (i.e. zero out column fields that are not arrived which is critical if used in a way when LidarScan object is reused.)

NOTE[pb]: in Python it’s almost always the new LidarScan is created from

scratch and used as a receiver of lidar packet in the batching implementation, thus finalization with zeros and a proper cut can be skipped, however it’s a huge difference from C++ batching loop impl and it’s important to keep things closer to C++ and also have a normal way to cut the very last LidarScan in a streams.

Parameters:
  • info (SensorInfo) – metadata of the current batcher that is in use

  • last_buf – the last buffer that was passed to batcher.

Return type:

LidarPacket

packets_to_scan(lidar_packets, info, *, fields=None)[source]

Batch buffers that belongs to a single scan into a LidarScan object.

Errors if lidar_packets buffers do not belong to a single LidarScan. Typically inconsistent measurement_ids or frame_ids in buffers is an error, as well as more buffers then a single LidarScan of a specified PacketFormat can take.

Return type:

LidarScan

cut_raw32_words(ls)[source]
Return type:

LidarScan

ouster.sdk.util.pose_util

no_scipy()[source]

Checks the scipy availability with a warning message.

Return type:

bool

normalize_vector(v)[source]
Return type:

ndarray

exp_rot_vec(vec)[source]

Converts so3 vector to a rotation matrix.

Parameters:

vec (ndarray) – so3 rotation vector [3] or vectors [N, 3] to rotation matrix [3, 3] or matrices [N, 3, 3]

Return type:

ndarray

Returns:

rotation matrix or matrices

log_rot_mat(rm)[source]

Convert rotation matrix to so3 coordinates (i.e. log() operator)

Parameters:

rm (ndarray) – rotation matrix [3, 3] or matrices [N, 3, 3]

Return type:

ndarray

Returns:

so3 coordinate rotation vector [3] or [N, 3]

exp_pose6(pose6)[source]

Convert exponential poses to homogeneous matrix poses.

Parameters:

pose6 (ndarray) – vector [6] or matrix [N, 6] of exponential poses

Return type:

ndarray

Returns:

Homogeneous matrix poses of size [4, 4] or [N, 4, 4].

log_pose(pose)[source]

Convert homogeneous matrix(s) to exp pose coordinates.

Parameters:

pose (ndarray) – homogeneous pose [4, 4] or poses [N, 4, 4]

Return type:

ndarray

Returns:

exp pose coordinates [6] or [N, 6]

pose_interp(p1, p2, t, *, delta_pose6=None)[source]

Pose interpolation between pose1 and pose2 at time t as ratio.

Parameters:
  • p1 (ndarray) – starting pose

  • p2 (ndarray) – ending pose

  • t (float) – ratio between pose p1 and p2 at what point to interpolate, not restricted between [0, 1] and can be extended for out of bounds

  • delta_pose6 (Optional[ndarray]) – pre-calculated difference inv(p1) @ p2, saves computation if it’s available already

Return type:

ndarray

Returns:

pose of the point at time t on the line defined by p1 and p2 on SE3 manifold

traj_interp(traj_poses, ts)[source]

Trajectory interpolation for points in between.

TODO[pb]: Extend with time_bounds args for traj evaluator when needed

Return type:

ndarray

class Poser(*args, **kwargs)[source]

Bases: Protocol

Actor that adds poses to LidarScans

class TrajectoryEvaluator(poses, *, time_bounds=0)[source]

Bases: Poser

Interpolates trajectory for a set of timestamps from knot poses.

TODO[pb]: Add function to add/remove knot poses from traj eval.

TODO: Optionally, we may want to implement these calculations in C++ and

use bindings to make it faster.

Parameters:
  • poses (Sequence[Tuple[Union[int, float, number], ndarray]]) – List of knot poses with timestamps. Every list item is a tuple (ts, pose).

  • time_bounds (Optional[float]) –

    whether to restrict the pose interpolation to the timestamp range within the poses list: None - no restriction at all on the timestamps that can

    be used to get pose from the trajectory

    0 - strict bounds on the timestamp range in the

    poses list

    >0 - ratio that is allowed to go over the timestamp

    bounds. ratio value is applied as the ratio of pose[1].ts - pose[0].ts for the left bound, and pose[N].ts - pose[N-1].ts for the right bound.

pose_at(ts)[source]

Calculates a single pose (4x4 matrix) at a given ts timestamp.

Return type:

ndarray

poses_at(ts)[source]

Calculates multiple poses (4x4 matrices) at a given ts timestamps.

Return type:

ndarray

get_rot_matrix_to_align_to_gravity(accel_x, accel_y, accel_z)[source]

Computes the rotation matrix needed to align a given acceleration vector with the direction of gravity, fixing the yaw angle to zero.

Parameters:
  • accel_x (float) – x-component of the acceleration vector.

  • accel_y (float) – y-component of the acceleration vector.

  • accel_z (float) – z-component of the acceleration vector.

Returns:

A 3x3 rotation matrix that aligns the acceleration vector with the gravity vector [0,0,1] while fixing the yaw angle to zero.

pose_scans(source, *, poses=None)[source]

Add poses to LidarScans stream.

Parameters:

source – one of: - Sequence[core.LidarScan] - single scan sources - Sequence[List[Optional[core.LidarScan]]] - multi scans sources

load_kitti_poses(file)[source]

Loads the Kitti poses from the file.

Return type:

ndarray

Returns:

[N, 4, 4] array of homogeneous poses

make_kiss_traj_poses(poses)[source]

Makes a traj poses from kiss poses.

Parameters:

poses (Union[Sequence[ndarray], ndarray]) – pose for every scan in the sequence as returned by KissICP

Returns:

0.5 For example scan indexes 0, 1, 2 produce timestamps 0.5, 1.5, 2.5

Return type:

trajectory poses timestamped by the scan index mid point

pose_scans_from_kitti(source, kitti_poses)[source]

Add poses to LidarScans stream using the previously saved per scan poses.

Every pose is considered to be in the middle of the scan. We assume that very first scan starts at t = 0 and ends at t = 1, thus the first pose is timestamped as 0.5, second pose is timestamped at 1.5 (middle of the second scan), and so on … to the very last pose N which timestamped at N + 0.5 for the last N scan.

Parameters:
  • source – one of: - Sequence[core.LidarScan] - single scan sources - Sequence[List[Optional[core.LidarScan]]] - multi scans sources

  • kitti_poses (str) – path to the file with in kitti poses format, i.e. every line contains 12 floats of 4x4 homogeneous transformation matrix ([:3, :] in numpy notation, row-major serialized)

ouster.sdk.util.progress_bar

progressbar(progress, total, prefix='', suffix='')[source]

Displays progress in the console as a percentage.

Parameters:
  • progress – The current progress (number of items completed).

  • total – The total number of items.

  • prefix – A prefix string to display before the progress bar (optional).

  • suffix – A suffix string to display after the progress bar (optional).