meta_streaming_info.h

ChunkInfo

struct ChunkInfo

Class for keeping track of OSF chunks.

Flat Buffer Reference: fb/streaming/streaming_info.fbs :: ChunkInfo

Public Members

uint64_t offset

The offset in the flatbuffer where the chunk is located.

Flat Buffer Reference: fb/streaming/streaming_info.fbs :: ChunkInfo :: offset

uint32_t stream_id

The specific stream the chunk is associated with.

Flat Buffer Reference: fb/streaming/streaming_info.fbs :: ChunkInfo :: stream_id

uint32_t message_count

The number of messages in the chunk

Flat Buffer Reference: fb/streaming/streaming_info.fbs :: ChunkInfo :: message_count

std::string ouster::osf::to_string(const ChunkInfo &chunk_info)

Get the string representation for a ChunkInfo object.

Parameters:

chunk_info – [in] ChunkInfo object to be converted to string

Returns:

The string representation for a ChunkInfo object.

StreamStats

struct StreamStats

Class for keeping track of OSF stream stats.

Flat Buffer Reference: fb/streaming/streaming_info.fbs :: StreamStats

Public Functions

StreamStats() = default

Default constructor, sets everthing to 0.

StreamStats(uint32_t s_id, ts_t receive_ts, ts_t sensor_ts, uint32_t msg_size)

Construct a StreamStats with the specified values

Parameters:
  • s_id – [in] Specify the stream_id to use.

  • receive_ts – [in] Set the start and end timestamps to the specified value and add it to the receive timestamps.

  • sensor_ts – [in] Add to the sensor timestamps.

  • msg_size – [in] Set the average message size to the specified value.

void update(ts_t receive_ts, ts_t sensor_ts, uint32_t msg_size)

Update values within the StreamStats

Parameters:
  • receive_ts – [in] Add another receive timestamp and calculate the start and end values.

  • sensor_ts – [in] Add another sensor timestamp

  • msg_size – [in] Add another message size and calculate the average.

Public Members

uint32_t stream_id

The specific stream the chunk is associated with.

Flat Buffer Reference: fb/streaming/streaming_info.fbs :: StreamStats :: stream_id

ts_t start_ts

The first timestamp in the stream.

Flat Buffer Reference: fb/streaming/streaming_info.fbs :: StreamStats :: start_ts

ts_t end_ts

The last timestamp in the stream.

Flat Buffer Reference: fb/streaming/streaming_info.fbs :: StreamStats :: end_ts

uint64_t message_count

The number of messages in the stream.

Flat Buffer Reference: fb/streaming/streaming_info.fbs :: StreamStats :: message_count

uint32_t message_avg_size

The average size of the messages in the stream.

Flat Buffer Reference: fb/streaming/streaming_info.fbs :: StreamStats :: message_avg_size

std::vector<uint64_t> receive_timestamps

The receive timestamps of each message in the stream.

Flat Buffer Reference: fb/streaming/streaming_info.fbs :: StreamStats :: receive_timestamps

std::vector<uint64_t> sensor_timestamps

The sensor timestamps of each message in the stream.

Flat Buffer Reference: fb/streaming/streaming_info.fbs :: StreamStats :: sensor_timestamps

std::string ouster::osf::to_string(const StreamStats &stream_stats)

Get the string representation for a StreamStats object.

Parameters:

stream_stats – [in] StreamStats object to be converted to string.

Returns:

The string representation for a StreamStats object.

Streaming Info

class StreamingInfo : public ouster::osf::MetadataEntryHelper<StreamingInfo>

Metadata entry to store StreamingInfo, to support StreamingLayout (RFC 0018)

OSF type: ouster/v1/streaming/StreamingInfo

Flat Buffer Reference: fb/streaming/streaming_info.fbs :: StreamingInfo

Public Functions

StreamingInfo(const std::vector<std::pair<uint64_t, ChunkInfo>> &chunks_info, const std::vector<std::pair<uint32_t, StreamStats>> &stream_stats)
Parameters:
  • chunks_info – [in] Vector containing pairs of stream_id/ChunkInfo to be used to generate a stream_id/ChunkInfo map.

  • stream_stats – [in] Vector containing pairs of stream_id/StreamStats to be used to generate a stream_id/StreamStats map.

StreamingInfo(const std::map<uint64_t, ChunkInfo> &chunks_info, const std::map<uint32_t, StreamStats> &stream_stats)
Parameters:
  • chunks_info – [in] ///< Map containing stream_id/ChunkInfo data.

  • stream_stats – [in] ///< Map containing stream_id/StreamStats data.

std::map<uint64_t, ChunkInfo> &chunks_info()

Return the chunk_info map. stream_id/ChunkInfo data.

Returns:

The chunk_info map. stream_id/ChunkInfo data.

std::map<uint32_t, StreamStats> &stream_stats()

Return the stream stat map. stream_id/StreamStats data.

Returns:

The stream stat map. stream_id/StreamStats data.

virtual std::vector<uint8_t> buffer() const final override

Byte represantation of the internal derived metadata type, used as serialization function when saving to OSF file.

Returns:

The byte vector representation of the metadata.

static std::unique_ptr<MetadataEntry> from_buffer(const std::vector<uint8_t> &buf)

Create a StreamingInfo object from a byte array.

Todo:

Figure out why this wasnt just done as a constructor overload.

Parameters:

buf – [in] The raw flatbuffer byte vector to initialize from.

Returns:

The new StreamingInfo cast as a MetadataEntry

virtual std::string repr() const override

Get the string representation for the LidarSensor object.

Returns:

The string representation for the LidarSensor object.

template<>
struct MetadataTraits<StreamingInfo>
#include <meta_streaming_info.h>

Templated struct for returning the OSF type string.

Public Static Functions

static inline const std::string type()

Return the OSF type string.

Returns:

The OSF type string “ouster/v1/streaming/StreamingInfo”.