meta_lidar_sensor.h

class LidarSensor : public ouster::osf::MetadataEntryHelper<LidarSensor>

Metadata entry to store lidar sensor_info, i.e. Ouster sensor configuration.

OSF type: ouster/v1/os_sensor/LidarSensor

Flat Buffer Reference: fb/os_sensor/lidar_sensor.fbs

Public Functions

explicit LidarSensor(const sensor_info &si)
Parameters:

si – [in] Initialize the LidarSensor with a sensor_info object.

explicit LidarSensor(const std::string &sensor_metadata)
Parameters:

sensor_metadata – [in] Initialize the LidarSensor with a json string representation of the sensor_info object.

const sensor_info &info() const

Returns the sensor_info associated with the LidarSensor.

Returns:

The sensor_info associated with the LidarSensor.

const std::string &metadata() const

Returns the json string representation sensor_info associated with the LidarSensor.

Returns:

///< The json string representation of the ///< sensor_info object.

virtual std::vector<uint8_t> buffer() const final

Byte represantation of the internal derived metadata type, used as serialization function when saving to OSF file.

Returns:

The byte vector representation of the metadata.

static std::unique_ptr<MetadataEntry> from_buffer(const std::vector<uint8_t> &buf)

Create a LidarSensor object from a byte array.

Todo:

Figure out why this wasnt just done as a constructor overload.

Parameters:

buf – [in] The raw flatbuffer byte vector to initialize from.

Returns:

The new LidarSensor cast as a MetadataEntry

virtual std::string repr() const override

Get the string representation for the LidarSensor object.

Returns:

The string representation for the LidarSensor object.

virtual std::string to_string() const override

Todo:

Figure out why we have both repr and to_string

Get the string representation for the LidarSensor object.

Returns:

The string representation for the LidarSensor object.

template<>
struct MetadataTraits<LidarSensor>
#include <meta_lidar_sensor.h>

Templated struct for returning the OSF type string.

Public Static Functions

static inline const std::string type()

Return the OSF type string.

Returns:

The OSF type string “ouster/v1/os_sensor/LidarSensor”.