types.h

Type-defs

template<typename T>
using ouster::img_t = Eigen::Array<T, -1, -1, Eigen::RowMajor>

For image operations.

Template Parameters

T – The data type for the array.

using ouster::mat4d = Eigen::Matrix<double, 4, 4, Eigen::DontAlign>

Used for transformations.

using ouster::sensor::AzimuthWindow = std::pair<int, int>

Convenience type alias for azimuth windows, the window over which the sensor fires in millidegrees.

using ouster::sensor::ColumnWindow = std::pair<int, int>

Convenience type alias for column windows, the window over which the sensor fires in columns.

Helper Data

Lidar Mode

enum ouster::sensor::lidar_mode

Constants used for configuration. Refer to the sensor documentation for the meaning of each option.

Values:

enumerator MODE_UNSPEC

lidar mode: unspecified

enumerator MODE_512x10

lidar mode: 10 scans of 512 columns per second

enumerator MODE_512x20

lidar mode: 20 scans of 512 columns per second

enumerator MODE_1024x10

lidar mode: 10 scans of 1024 columns per second

enumerator MODE_1024x20

lidar mode: 20 scans of 1024 columsn per second

enumerator MODE_2048x10

lidar mode: 10 scans of 2048 columns per second

enumerator MODE_4096x5

lidar mode: 5 scans of 4096 columns per second. Only available on select sensors

uint32_t ouster::sensor::n_cols_of_lidar_mode(lidar_mode mode)

Get number of columns in a scan for a lidar mode.

Parameters

mode – [in] lidar_mode to get the number of columns for.

Returns

number of columns per rotation for the mode.

int ouster::sensor::frequency_of_lidar_mode(lidar_mode mode)

Get the lidar rotation frequency from lidar mode.

Parameters

mode – [in] Lidar mode to get the rotation frequency from.

Returns

lidar rotation frequency in Hz.

std::string ouster::sensor::to_string(lidar_mode mode)

Get string representation of a lidar mode.

Parameters

mode – [in] lidar_mode to get the string representation for.

Returns

string representation of the lidar mode, or “UNKNOWN”.

lidar_mode ouster::sensor::lidar_mode_of_string(const std::string &s)

Get lidar mode from string.

Parameters

s – [in] String to decode.

Returns

lidar mode corresponding to the string, or 0 on error.

Timestamp Mode

enum ouster::sensor::timestamp_mode

Mode controlling timestamp method. Refer to the sensor documentation for the meaning of each option.

Values:

enumerator TIME_FROM_UNSPEC

Timestamp mode unspecified.

enumerator TIME_FROM_INTERNAL_OSC

Use the internal clock.

enumerator TIME_FROM_SYNC_PULSE_IN

A free running counter synced to the SYNC_PULSE_IN input counts seconds (# of pulses) and nanoseconds since sensor turn on.

enumerator TIME_FROM_PTP_1588

Synchronize with an external PTP master.

std::string ouster::sensor::to_string(timestamp_mode mode)

Get string representation of a timestamp mode.

Parameters

mode – [in] timestamp_mode to get the string representation for.

Returns

string representation of the timestamp mode, or “UNKNOWN”.

timestamp_mode ouster::sensor::timestamp_mode_of_string(const std::string &s)

Get timestamp mode from string.

Parameters

s – [in] String to decode into a timestamp mode.

Returns

timestamp mode corresponding to the string, or 0 on error.

Operating Mode

enum ouster::sensor::OperatingMode

Mode controlling sensor operation. Refer to the sensor documentation for the meaning of each option.

Values:

enumerator OPERATING_NORMAL

Normal sensor operation.

enumerator OPERATING_STANDBY

Standby.

std::string ouster::sensor::to_string(OperatingMode mode)

Get string representation of an operating mode.

Parameters

mode – [in] Operating mode to get the string representation from.

Returns

string representation of the operating mode, or “UNKNOWN”.

optional<OperatingMode> ouster::sensor::operating_mode_of_string(const std::string &s)

Get operating mode from string.

Parameters

s – String to get the operating mode from.

Returns

operating mode corresponding to the string, or 0 on error.

Multipurpose IO Mode

enum ouster::sensor::MultipurposeIOMode

Mode controlling ways to input timesync information. Refer to the sensor documentation for the meaning of each option.

Values:

enumerator MULTIPURPOSE_OFF

Multipurpose IO is turned off (default)

enumerator MULTIPURPOSE_INPUT_NMEA_UART

Used in conjunction with timestamp_mode::TIME_FROM_SYNC_PULSE_IN to enable time pulses in on the multipurpose io input.

enumerator MULTIPURPOSE_OUTPUT_FROM_INTERNAL_OSC

Output a SYNC_PULSE_OUT signal synchronized with the internal clock.

enumerator MULTIPURPOSE_OUTPUT_FROM_SYNC_PULSE_IN

Output a SYNC_PULSE_OUT signal synchronized with a SYNC_PULSE_IN provided to the unit.

enumerator MULTIPURPOSE_OUTPUT_FROM_PTP_1588

Output a SYNC_PULSE_OUT signal synchronized with an external PTP IEEE 1588 master.

enumerator MULTIPURPOSE_OUTPUT_FROM_ENCODER_ANGLE

Output a SYNC_PULSE_OUT signal with a user defined rate in an integer number of degrees.

std::string ouster::sensor::to_string(MultipurposeIOMode mode)

Get string representation of a multipurpose io mode.

Parameters

mode – [in] Multipurpose io mode to get a string representation from.

Returns

string representation of the multipurpose io mode, or “UNKNOWN”.

optional<MultipurposeIOMode> ouster::sensor::multipurpose_io_mode_of_string(const std::string &s)

Get multipurpose io mode from string.

Parameters

s – [in] String to decode into a multipurpose io mode.

Returns

multipurpose io mode corresponding to the string, or 0 on error.

Polarity

enum ouster::sensor::Polarity

Polarity represents polarity of NMEA UART and SYNC_PULSE inputs and outputs. See sensor docs for more details.

Values:

enumerator POLARITY_ACTIVE_LOW

ACTIVE_LOW.

enumerator POLARITY_ACTIVE_HIGH

ACTIVE_HIGH.

std::string ouster::sensor::to_string(Polarity polarity)

Get string representation of a polarity.

Parameters

polarity – [in] The polarity to get the string representation of.

Returns

string representation of the polarity, or “UNKNOWN”.

optional<Polarity> ouster::sensor::polarity_of_string(const std::string &s)

Get polarity from string.

Parameters

s – [in] The string to decode into a polarity.

Returns

polarity corresponding to the string, or 0 on error.

NMEA Baud Rate

enum ouster::sensor::NMEABaudRate

Baud rate the sensor attempts for NMEA UART input $GPRMC messages See sensor docs for more details.

Values:

enumerator BAUD_9600

9600 bits per second UART baud rate

enumerator BAUD_115200

115200 bits per second UART baud rate

std::string ouster::sensor::to_string(NMEABaudRate rate)

Get string representation of a NMEA Baud Rate.

Parameters

rate – [in] The NNEABaudRate to get the string representation of.

Returns

string representation of the NMEA baud rate, or “UNKNOWN”.

optional<NMEABaudRate> ouster::sensor::nmea_baud_rate_of_string(const std::string &s)

Get nmea baud rate from string.

Parameters

s – [in] The string to decode into a NMEA baud rate.

Returns

nmea baud rate corresponding to the string, or 0 on error.

UDP Profile Lidar

enum ouster::sensor::UDPProfileLidar

Profile indicating packet format of lidar data.

Values:

enumerator PROFILE_LIDAR_UNKNOWN
enumerator PROFILE_LIDAR_LEGACY

Legacy lidar data

enumerator PROFILE_RNG19_RFL8_SIG16_NIR16_DUAL

Dual Returns data

enumerator PROFILE_RNG19_RFL8_SIG16_NIR16

Single Returns data

enumerator PROFILE_RNG15_RFL8_NIR8

Single Returns Low Data Rate

enumerator PROFILE_FIVE_WORD_PIXEL

Five Word Profile

enumerator PROFILE_FUSA_RNG15_RFL8_NIR8_DUAL

FuSa two-word pixel

std::string ouster::sensor::to_string(UDPProfileLidar profile)

Get string representation of a lidar profile.

Parameters

profile – [in] The profile to get the string representation of.

Returns

string representation of the lidar profile.

optional<UDPProfileLidar> ouster::sensor::udp_profile_lidar_of_string(const std::string &s)

Get lidar profile from string.

Parameters

s – [in] The string to decode into a lidar profile.

Returns

lidar profile corresponding to the string, or nullopt on error.

UDP Profile IMU

enum ouster::sensor::UDPProfileIMU

Profile indicating packet format of IMU data.

Values:

enumerator PROFILE_IMU_LEGACY

Legacy IMU data.

std::string ouster::sensor::to_string(UDPProfileIMU profile)

Get string representation of an IMU profile.

Parameters

profile – [in] The profile to get the string representation of.

Returns

string representation of the lidar profile.

optional<UDPProfileIMU> ouster::sensor::udp_profile_imu_of_string(const std::string &s)

Get imu profile from string

Parameters

s – [in] The string to decode into an imu profile.

Returns

imu profile corresponding to the string, or nullopt on error.

Chan Field

enum ouster::sensor::ChanFieldType

Types of channel fields.

Values:

enumerator VOID
enumerator UINT8
enumerator UINT16
enumerator UINT32
enumerator UINT64
enum ouster::sensor::ChanField

Tag to identitify a paricular value reported in the sensor channel data block.

Values:

enumerator RANGE

1st return range in mm

enumerator RANGE2

2nd return range in mm

enumerator INTENSITY

Deprecated:

Use SIGNAL instead

enumerator SIGNAL

1st return signal in photons

enumerator SIGNAL2

2nd return signal in photons

enumerator REFLECTIVITY

1st return reflectivity, calibrated by range and sensor sensitivity in FW 2.1+. See sensor docs for more details

enumerator REFLECTIVITY2

2nd return reflectivity, calibrated by range and sensor sensitivity in FW 2.1+. See sensor docs for more details

enumerator AMBIENT

Deprecated:

Use NEAR_IR instead

enumerator NEAR_IR

near_ir in photons

enumerator FLAGS

1st return flags

enumerator FLAGS2

2nd return flags

enumerator RAW_HEADERS

raw headers for packet/footer/column for dev use

enumerator RAW32_WORD5

raw word access to packet for dev use

enumerator RAW32_WORD6

raw word access to packet for dev use

enumerator RAW32_WORD7

raw word access to packet for dev use

enumerator RAW32_WORD8

raw word access to packet for dev use

enumerator RAW32_WORD9

raw word access to packet for dev use

enumerator CUSTOM0

custom user field

enumerator CUSTOM1

custom user field

enumerator CUSTOM2

custom user field

enumerator CUSTOM3

custom user field

enumerator CUSTOM4

custom user field

enumerator CUSTOM5

custom user field

enumerator CUSTOM6

custom user field

enumerator CUSTOM7

custom user field

enumerator CUSTOM8

custom user field

enumerator CUSTOM9

custom user field

enumerator RAW32_WORD1

raw word access to packet for dev use

enumerator RAW32_WORD2

raw word access to packet for dev use

enumerator RAW32_WORD3

raw word access to packet for dev use

enumerator RAW32_WORD4

raw word access to packet for dev use

enumerator CHAN_FIELD_MAX

max which allows us to introduce future fields

std::string ouster::sensor::to_string(ChanField field)

Get string representation of a channel field.

Parameters

field – [in] The field to get the string representation of.

Returns

string representation of the channel field.

Sensor Info

struct ouster::sensor::sensor_info

Stores parsed information from metadata and

Public Members

std::string name = {}

user-convenience client-side assignable name, corresponds to hostname in metadata.json if present

std::string sn = {}

sensor serial number corresponding to prod_sn in metadata.json

std::string fw_rev = {}

fw revision corresponding to build_rev in metadata.json

lidar_mode mode = {}

lidar mode of sensor

std::string prod_line = {}

prod line

data_format format = {}

data format of sensor

std::vector<double> beam_azimuth_angles = {}

beam azimuth angles for 3D projection

std::vector<double> beam_altitude_angles = {}

beam altitude angles for 3D projection

double lidar_origin_to_beam_origin_mm = {}

distance between lidar origin and beam origin in mm

mat4d beam_to_lidar_transform = mat4d::Zero()

transform between beam and lidar frame

mat4d imu_to_sensor_transform = mat4d::Zero()

transform between sensor coordinate frame and imu

mat4d lidar_to_sensor_transform = mat4d::Zero()

transform between lidar and sensor coordinate frames

mat4d extrinsic = mat4d::Zero()

user-convenience client-side assignable extrinsic matrix, currently is not read from metadata.json

uint32_t init_id = {}

initialization ID updated every reinit

uint16_t udp_port_lidar = {}

the lidar destination port

uint16_t udp_port_imu = {}

the imu destination port

std::string build_date = {}

build date from FW sensor_info

std::string image_rev = {}

image rev from FW sensor_info

std::string prod_pn = {}

prod pn

std::string status = {}

sensor status at time of pulling metadata

calibration_status cal = {}

sensor calibration

sensor_config config = {}

parsed sensor config if available from metadata

sensor_info ouster::sensor::default_sensor_info(lidar_mode mode)

Get a default sensor_info for the given lidar mode.

Parameters

mode – [in] lidar mode to generate default sensor_info for.

Returns

default sensor_info for the OS1-64.

sensor_info ouster::sensor::parse_metadata(const std::string &metadata, bool skip_beam_validation = false)

Parse metadata text blob from the sensor into a sensor_info struct.

String and vector fields will have size 0 if the parameter cannot be found or parsed, while lidar_mode will be set to 0 (invalid).

Throws

runtime_error – if the text is not valid json

Parameters
  • metadata – [in] a text blob returned by get_metadata from client.h.

  • skip_beam_validation – [in] whether to skip validation on metdata - not for use on recorded data or metadata from sensors

Returns

a sensor_info struct populated with a subset of the metadata.

sensor_info ouster::sensor::metadata_from_json(const std::string &json_file, bool skip_beam_validation = false)

Parse metadata given path to a json file.

Throws

runtime_error – if json file does not exist or is malformed.

Parameters
  • json_file – [in] path to a json file containing sensor metadata.

  • skip_beam_validation – [in] whether to skip validation on metadata - not for use on recorded data or metadata from sensors

Returns

a sensor_info struct populated with a subset of the metadata.

std::string ouster::sensor::convert_to_legacy(const std::string &metadata)

Convert non-legacy string representation of metadata to legacy.

Parameters

metadata – [in] non-legacy string representation of metadata.

Returns

legacy string representation of metadata.

bool ouster::sensor::operator==(const sensor_info &lhs, const sensor_info &rhs)

Equality for sensor_info.

Parameters
  • lhs – [in] The first object to compare.

  • rhs – [in] The second object to compare.

Returns

lhs == rhs

bool ouster::sensor::operator!=(const sensor_info &lhs, const sensor_info &rhs)

Not-Equality for sensor_info.

Parameters
  • lhs – [in] The first object to compare.

  • rhs – [in] The second object to compare.

Returns

lhs != rhs

std::string ouster::sensor::to_string(const sensor_info &info)

String representation of the sensor_info. All fields included. NOT equivalent or interchangeable with metadata from sensor.

Parameters

info – [in] sensor_info struct

Returns

a debug string in json format

Sensor Config

struct ouster::sensor::sensor_config

Struct for sensor configuration parameters.

Public Members

optional<std::string> udp_dest

The destination address for the lidar/imu data to be sent to

optional<int> udp_port_lidar

The destination port for the lidar data to be sent to

optional<int> udp_port_imu

The destination port for the imu data to be sent to

optional<timestamp_mode> ts_mode

The timestamp mode for the sensor to use. Refer to timestamp_mode for more details.

optional<lidar_mode> ld_mode

The lidar mode for the sensor to use. Refer to lidar_mode for more details.

optional<OperatingMode> operating_mode

The operating mode for the sensor to use. Refer to OperatingMode for more details.

optional<MultipurposeIOMode> multipurpose_io_mode

The multipurpose io mode for the sensor to use. Refer to MultipurposeIOMode for more details.

optional<AzimuthWindow> azimuth_window

The azimuth window for the sensor to use. Refer to AzimuthWindow for more details.

optional<double> signal_multiplier

Multiplier for signal strength of sensor. See the sensor docs for more details on usage.

optional<Polarity> nmea_in_polarity

The nmea polarity for the sensor to use. Refer to Polarity for more details.

optional<bool> nmea_ignore_valid_char

Whether NMEA UART input $GPRMC messages should be ignored. Refer to the sensor docs for more details.

optional<NMEABaudRate> nmea_baud_rate

The nmea baud rate for the sensor to use. Refer to Polarity> for more details.

optional<int> nmea_leap_seconds

Number of leap seconds added to UDP timestamp. See the sensor docs for more details.

optional<Polarity> sync_pulse_in_polarity

Polarity of SYNC_PULSE_IN input. See Polarity for more details.

optional<Polarity> sync_pulse_out_polarity

Polarity of SYNC_PULSE_OUT output. See Polarity for more details.

optional<int> sync_pulse_out_angle

Angle in degrees that sensor traverses between each SYNC_PULSE_OUT pulse. See senor docs for more details.

optional<int> sync_pulse_out_pulse_width

Width of SYNC_PULSE_OUT pulse in ms. See sensor docs for more details.

optional<int> sync_pulse_out_frequency

Frequency of SYNC_PULSE_OUT pulse in Hz. See sensor docs for more details.

optional<bool> phase_lock_enable

Whether phase locking is enabled. See sensor docs for more details.

optional<int> phase_lock_offset

Angle that sensors are locked to in millidegrees. See sensor docs for more details.

optional<int> columns_per_packet

Columns per packet. See sensor docs for more details.

optional<UDPProfileLidar> udp_profile_lidar

The lidar profile for the sensor to use. Refer to UDPProfileLidar for more details.

optional<UDPProfileIMU> udp_profile_imu

The imu profile for the sensor to use. Refer to UDPProfileIMU for more details.

sensor_config ouster::sensor::parse_config(const std::string &config)

Parse config text blob from the sensor into a sensor_config struct.

All fields are optional, and will only be set if found.

Throws

runtime_error – if the text is not valid json.

Parameters

config – [in] a text blob given by get_config from client.h.

Returns

a sensor_config struct populated with the sensor config. parameters.

bool ouster::sensor::operator==(const sensor_config &lhs, const sensor_config &rhs)

Equality for sensor config.

Parameters
  • lhs – [in] The first object to compare.

  • rhs – [in] The second object to compare.

Returns

lhs == rhs

bool ouster::sensor::operator!=(const sensor_config &lhs, const sensor_config &rhs)

Not-Equality for sensor config.

Parameters
  • lhs – [in] The first object to compare.

  • rhs – [in] The second object to compare.

Returns

lhs != rhs

std::string ouster::sensor::to_string(const sensor_config &config)

Get a string representation of sensor config. Only set fields will be represented.

Parameters

config – [in] a struct of sensor config.

Returns

a json sensor config string.

Data Format

struct ouster::sensor::data_format

Stores data format information.

Public Members

uint32_t pixels_per_column

pixels per column

uint32_t columns_per_packet

columns per packet

uint32_t columns_per_frame

columns per frame, should match with lidar mode

std::vector<int> pixel_shift_by_row

shift of pixels by row to enable destagger

ColumnWindow column_window

window of columns over which sensor fires

UDPProfileLidar udp_profile_lidar = {}

profile of lidar packet

UDPProfileIMU udp_profile_imu = {}

profile of imu packet

uint16_t fps

frames per second

bool ouster::sensor::operator==(const data_format &lhs, const data_format &rhs)

Equality for data_format.

Parameters
  • lhs – [in] The first object to compare.

  • rhs – [in] The second object to compare.

Returns

lhs == rhs

bool ouster::sensor::operator!=(const data_format &lhs, const data_format &rhs)

Not-Equality for data_format.

Parameters
  • lhs – [in] The first object to compare.

  • rhs – [in] The second object to compare.

Returns

lhs != rhs

Packet Format

class ouster::sensor::packet_format

Table of accessors for extracting data from imu and lidar packets.

In the user guide, refer to section 9 for the lidar packet format and section 10 for imu packets.

For 0 <= n < columns_per_packet, nth_col(n, packet_buf) returns a pointer to the nth measurement block. For 0 <= m < pixels_per_column, nth_px(m, col_buf) returns the mth channel data block.

Use imu_la_{x,y,z} to access the acceleration in the corresponding direction. Use imu_av_{x,y,z} to read the angular velocity.

Subclassed by ouster::sensor::impl::packet_writer

Public Types

FieldIter = decltype(field_types_)::const_iterator

iterator over field types of packet

Public Functions

uint16_t packet_type(const uint8_t *lidar_buf) const

Read the packet type packet header.

Parameters

lidar_buf – [in] the lidar buf.

Returns

the packet type.

uint32_t frame_id(const uint8_t *lidar_buf) const

Read the frame_id packet header.

Parameters

lidar_buf – [in] the lidar buf.

Returns

the frame id.

uint32_t init_id(const uint8_t *lidar_buf) const

Read the initialization id packet header.

Parameters

lidar_buf – [in] the lidar buf.

Returns

the init id.

uint64_t prod_sn(const uint8_t *lidar_buf) const

Read the packet serial number header.

Parameters

lidar_buf – [in] the lidar buf.

Returns

the serial number.

uint16_t countdown_thermal_shutdown(const uint8_t *lidar_buf) const

Read the packet thermal shutdown countdown

Parameters

lidar_buf – [in] the lidar buf.

Returns

the thermal shutdown countdown.

uint16_t countdown_shot_limiting(const uint8_t *lidar_buf) const

Read the packet shot limiting countdown

Parameters

lidar_buf – [in] the lidar buf.

Returns

the shot limiting countdown.

uint8_t thermal_shutdown(const uint8_t *lidar_buf) const

Read the packet thermal shutdown header.

Parameters

lidar_buf – [in] the lidar buf.

Returns

the thermal shutdown status

uint8_t shot_limiting(const uint8_t *lidar_buf) const

Read the packet shot limiting header.

Parameters

lidar_buf – [in] the lidar buf.

Returns

the shot limiting status

ChanFieldType field_type(ChanField f) const

Get the bit width of the specified channel field.

Parameters

f – [in] the channel field to query.

Returns

a type tag specifying the bitwidth of the requested field or ChannelFieldType::VOID if it is not supported by the packet format.

FieldIter begin() const

A const forward iterator over field / type pairs.

FieldIter end() const

A const forward iterator over field / type pairs.

const uint8_t *footer(const uint8_t *lidar_buf) const

Get pointer to the packet footer of a lidar buffer.

Parameters

lidar_buf – [in] the lidar buffer.

Returns

pointer to packet footer of lidar buffer, can be nullptr if packet format doesn’t have packet footer.

const uint8_t *nth_col(int n, const uint8_t *lidar_buf) const

Get pointer to nth column of a lidar buffer.

Parameters
  • n – [in] which column.

  • lidar_buf – [in] the lidar buffer.

Returns

pointer to nth column of lidar buffer.

uint64_t col_timestamp(const uint8_t *col_buf) const

Read column timestamp from column buffer.

Parameters

col_buf – [in] the column buffer.

Returns

column timestamp.

uint16_t col_measurement_id(const uint8_t *col_buf) const

Read measurement id from column buffer.

Parameters

col_buf – [in] the column buffer.

Returns

column measurement id.

uint32_t col_status(const uint8_t *col_buf) const

Read column status from column buffer.

Parameters

col_buf – [in] the column buffer.

Returns

column status.

uint32_t col_encoder(const uint8_t *col_buf) const

Deprecated:

Encoder count is deprecated as it is redundant with measurement id, barring a multiplication factor which varies by lidar mode. Use col_measurement_id instead

uint16_t col_frame_id(const uint8_t *col_buf) const

Deprecated:

Use frame_id instead

template<typename T, typename std::enable_if<std::is_unsigned<T>::value, T>::type = 0>
void col_field(const uint8_t *col_buf, ChanField f, T *dst, int dst_stride = 1) const

Copy the specified channel field out of a packet measurement block.

Template Parameters

T – T should be an unsigned integer type large enough to store values of the specified field. Otherwise, data will be truncated.

Parameters
  • col_buf – [in] a measurement block pointer returned by nth_col().

  • f – [in] the channel field to copy.

  • dst – [out] destination array of size pixels_per_column * dst_stride.

  • dst_stride – [in] stride for writing to the destination array.

int block_parsable() const

Returns maximum available size of parsing block usable with block_field

if packet format does not allow for block parsing, returns 0

template<typename T, int BlockDim, typename std::enable_if<std::is_unsigned<T>::value, T>::type = 0>
void block_field(Eigen::Ref<img_t<T>> field, ChanField f, const uint8_t *lidar_buf) const

Copy the specified channel field out of a packet measurement block. Faster traversal than col_field, but has to copy the entire packet all at once.

Template Parameters

T – T should be an unsigned integer type large enough to store values of the specified field. Otherwise, data will be truncated.

Parameters
  • field – [out] destination eigen array

  • f – [in] the channel field to copy.

  • lidar_buf – [in] the lidar buffer.

const uint8_t *nth_px(int n, const uint8_t *col_buf) const

Get pointer to nth pixel of a column buffer.

Parameters
  • n – [in] which pixel.

  • col_buf – [in] the column buffer.

Returns

pointer to nth pixel of a column buffer.

uint64_t imu_sys_ts(const uint8_t *imu_buf) const

Read sys ts from imu packet buffer.

Parameters

imu_buf – [in] the imu packet buffer.

Returns

sys ts from imu pacet buffer.

uint64_t imu_accel_ts(const uint8_t *imu_buf) const

Read acceleration timestamp.

Parameters

imu_buf – [in] the imu packet buffer.

Returns

acceleration ts from imu packet buffer.

uint64_t imu_gyro_ts(const uint8_t *imu_buf) const

Read gyro timestamp.

Parameters

imu_buf – [in] the imu packet buffer.

Returns

gyro ts from imu packet buffer.

float imu_la_x(const uint8_t *imu_buf) const

Read acceleration in x.

Parameters

imu_buf – [in] the imu packet buffer.

Returns

acceleration in x.

float imu_la_y(const uint8_t *imu_buf) const

Read acceleration in y.

Parameters

imu_buf – [in] the imu packet buffer.

Returns

acceleration in y.

float imu_la_z(const uint8_t *imu_buf) const

Read acceleration in z.

Parameters

imu_buf – [in] the imu packet buffer.

Returns

acceleration in z.

float imu_av_x(const uint8_t *imu_buf) const

Read angular velocity in x.

Parameters

imu_buf – [in] the imu packet buffer.

Returns

angular velocity in x.

float imu_av_y(const uint8_t *imu_buf) const

Read angular velocity in y.

Parameters

imu_buf – [in] the imu packet buffer.

Returns

angular velocity in y.

float imu_av_z(const uint8_t *imu_buf) const

Read angular velocity in z.

Parameters

imu_buf – [in] the imu packet buffer.

Returns

angular velocity in z.

uint64_t field_value_mask(ChanField f) const

Get the mask of possible values that can be parsed by the channel field

Parameters

f – [in] the channel field

Returns

mask of possible values

int field_bitness(ChanField f) const

Get number of bits in the channel field

Parameters

f – [in] the channel field

Returns

number of bits

Public Members

const UDPProfileLidar udp_profile_lidar

udp lidar profile of packet format

const size_t lidar_packet_size

lidar packet size

const size_t imu_packet_size

imu packet size

const int columns_per_packet

columns per lidar packet

const int pixels_per_column

pixels per column for lidar

struct Impl

Warning

doxygenfunction: Unable to resolve function “ouster::sensor::get_format” with arguments None in doxygen xml output for project “cpp_api” from directory: /sdk-extensions/docs/standard/build/ouster-sdk/doctrees/xml. Potential matches:

- const packet_format &get_format(UDPProfileLidar udp_profile_lidar, size_t pixels_per_column, size_t columns_per_packet)
- const packet_format &get_format(const sensor_info &info)

MISC

std::string ouster::sensor::client_version()

Get client version.

Returns

client version string

constexpr double ouster::sensor::range_unit = 0.001

Unit of range from sensor packet, in meters.