Appendix

Minimum Hardware Requirements

  • CPU: Intel Haswell (2013) or better.

  • Requires a CPU with 4 physical cores running at 1.5 Ghz, at least.

  • Requires a CPU running x86 or 64 instructions. No ARM support (except M1).

  • Requires at least 4-GB of RAM.

  • Requires appropriate network card to interface with the LiDARs: 1 Gigabit ethernet port.

  • A graphics card (for visualization part).

Compatible Operating Systems

  • Windows 10 (NOT tested on “Windows 10 on ARM”)

  • Ubuntu 18.04 and Ubuntu 20.04

  • Mac OS 10.11+

Limitations with Ouster Studio

  • Windows version is not signed and notarized.

  • Limited to visualizing and playing back dual return data but does not support multi-return color mode highlighting.

  • Not supported FW versions v2.2 or prior.

Supporting Documentation

The Ouster sensor documentation is meant to allow the users to take advantage of all the features that are available with Ouster Sensors.

Quick links:

Sample Data

Note

All Ouster sample data is provided under the CC BY-NC-SA license, whether obtained through the above links or from the Ouster website.

Visualize recorded data:

Changelog

Software v2.2.0

Date:

July 2025

Description:

“Added”

  • Share data with Ouster - Users can now share data with Ouster’s technical and customer support team for guidance and troubleshooting.

  • Support for large file uploads upto 100GB.

“Updated”

  • Resource optimization for processing bag files.

  • Consistency of color profiles between Ouster Studio Desktop (OSD) and Ouster Studio Web (OSW).

  • Improved playback speed while multiple 2D images are present.

“Fixed”

  • Issue with bag file processing.

  • Issue with switching between orthographic and perspective modes, and panning in orthographic mode.

Software v2.0.6

Date:

February 2025

Description:

“Added”

  • Local OSF File Replay – Support for replaying OSF files locally.

  • Cloud Integration – Enables cloud-based storage and management for seamless data access.

  • Latest Sample Data View – Users can now access the most recent sample data.

  • Authentication for Private Organizations, including:

    • Cloud Recording Management – Share, delete, upload, and download cloud recordings.

    • Visualization Tools – View and analyze cloud-stored recordings.

    • User Profile Management – Update user profile details.

    • Organization Management – Invite team members and configure access controls.

“Updated”

  • 2D Image Panel UI Enhancements

    • Improved usability with new navigation options.

    • Moved “Sample Data” and “Cloud Recording” options to the left sidebar.

    • “Sample Data” is now always visible, positioned next to “Home.”

  • UI Refinements

    • Updated the logo.

    • Merged “Feedback” and “Support” buttons into a user menu dropdown in the top-right corner.

Software v2.0.5

Date:

October 2024

Description:

“Added”

  • Download Data menu in cloud data tabs

  • Copyright footer on all screens

“Updated”

  • PCAP tab state persistence

  • Keyboard shortcuts modal

  • Top bar UI changes

“Fixed”

  • Fixed a bug where the right sidebar could be displayed on streamed data using a keyboard shortcut, despite being hidden

  • Implemented missing playback speed shortcuts for streamed data

“Removed”

  • Keyboard shortcuts button from the top bar unless on the visualization page

Software v2.0.4

Date:

July 2024

Description:

“Added”

  • Cloud tab has list of public sample data

  • Add orthographic camera toggle to left sidebar

  • Add orthographic camera toggle shortcut

  • Add frame index column to exported .CSV for .PCAP

“Fixed”

  • Fix bug where failed .CSV save still displayed success popup

Software v2.0.3

Date:

May 2024

Description:

“Added”

  • Compatibility with Firmware 3.1

  • Signed windows executable

“Improved”

  • Improved mDNS discovery

    • Explicitly requests followup records during service discovery for compatibility with earlier FW 3.1 release candidates

“Fixed”

  • Static IP setting update

    • Accepts plain IPv4 addresses, but warns user and will add /24 when sending request to sensor

    • Replaces /0 and /32 netmasks with /24

    • Studio 2.0.2 did not accept ipv4 addresses with netmasks included, this is fixed.

    • Fixed window sizing for static IP config popup hiding ‘Submit’ button

    • Keybindings and edit menu - cut, copy, paste, enter to submit

  • FW < 2.2 compatibility

    • Fixed bug for sensors running older fw (<2.2) not streaming data properly due to metadata missing udp_profile_lidar

    • Fixed bug where sensor lib attempted to send HTTP requests over port 7501

Software v2.0.2

Date:

October 2023

Description:

“Added”

  • Add support for FW 3.1

    • Support FUSA data profile

    • Support 4096x5 mode

  • Add fixed distance range rings to scene

    • Toggle visibility in ‘Scene’ tab

  • Enable static IP setting from sensor selection page

“Updated”

  • Update 2D image angle rulers

    • Shift range from [-180, 180] to [0, 360]

    • Match displayed angles to Lidar Coordinate Frame - 0 degrees is at the external connector, increasing counterclockwise from the connector.

Software v2.0.1

Date:

August 2023

Description:

“Added”

  • Pcap scrubbing

    • Can click/drag or use arrow keys to navigate through pcaps frame by frame

    • Enabled after indexing is completed

    • Navigating forward/backward by frame does not wrap and pauses the playback

  • Highlight pointclouds by return

    • Add UI element to left sidebar to select highlight colors per-return

  • Add ‘Invert Scene’ checkbox to left sidebar ‘Scene’ tab

    • Flips both pointcloud and 2D image for more convenient visualization of sensors mounted upside down such as the DOME

  • Move 2D Image controls to Left Sidebar ‘Scene’ Subsection

  • Add ability to opt out of autoupdates and manually check for updates

  • Record imu packets to pcap in addition to lidar packets

  • Add support for FW versions between 2.0-2.2

    • Communicate with sensors running FW <=2.2 over TCP interface

    • Communicate with sensors running FW >2.2 over HTTP

“Fixed”

  • Fix memory leak in data pipeline

    • Reduces lag in long-running application instances

  • Fix last frame visual glitch on first pcap play through

  • If sensor is in STANDBY when user clicks ‘Configure and Visualize’, set state to RUNNING

  • Allow only one app instance at a time

    • Fixes bug in Windows/Linux where a second app instance opens but playback fails

“Updated”

  • Improve responsiveness on external sensor configuration

    • Update ‘Scene’ tab’s visible returns when external sensor reconfig is detected

    • Change export tab to export both returns by default when available

  • Update selected sensor metadata more frequently on sensor selection page

Software v2.0.0

Date:

July 2023

Description:

Public Release